2024-03-14 9:58 AM
I create a project by selecting the NUCLEO-H563ZI and answer yes to the question about initializing peripherals and the project will not build. The error is:
file included from ../Drivers/STM32H5xx_HAL_Driver/Inc/stm32h5xx_hal.h:29,
from ../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_hal.c:35:
../Core/Inc/stm32h5xx_hal_conf.h:409:11: fatal error: stm32h5xx_hal_usart.h: No such file or directory
409 | #include "stm32h5xx_hal_usart.h"
| ^~~~~~~~~~~~~~~~~~~~~~~
The IDE reports itself to be
STM32CubeIDE
Version: 1.14.0
Build: 19471_20231121_1200 (UTC)
If I try to read the ioc file and generate code from the STM32CubeMX standalone the problem persists. CubeMX reports itself to be "Version 6.10.0"
I see others have reported similar problems, please provide some suggestions on the fix.
Solved! Go to Solution.
2024-03-14 10:27 AM - edited 2024-03-14 10:31 AM
Hello @MikeMcCormack and welcome to the ST Community :smiling_face_with_smiling_eyes:.
This is a confirmed issue on CubeMX and it is internally escalated under ticket number 171330.
(PS: ID 171330 is an internal tracking number and is not accessible or usable by customers).
So, as a workaround until correction on the next releases, i suggest you to comment the "#define HAL_USART_MODULE_ENABLED" if you are not configuring any USART and to comment "#define HAL_UART_MODULE_ENABLED" if you are not using any uart (or USART in asynchrone mode).
Ps: Those defines are on the stm32h5_xx_hal_conf.h file.
Then, the problem should be solved.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-03-14 10:06 AM
>> please provide some suggestions on the fix.
Copy the file from the repo into your project directories manually.
2024-03-14 10:27 AM - edited 2024-03-14 10:31 AM
Hello @MikeMcCormack and welcome to the ST Community :smiling_face_with_smiling_eyes:.
This is a confirmed issue on CubeMX and it is internally escalated under ticket number 171330.
(PS: ID 171330 is an internal tracking number and is not accessible or usable by customers).
So, as a workaround until correction on the next releases, i suggest you to comment the "#define HAL_USART_MODULE_ENABLED" if you are not configuring any USART and to comment "#define HAL_UART_MODULE_ENABLED" if you are not using any uart (or USART in asynchrone mode).
Ps: Those defines are on the stm32h5_xx_hal_conf.h file.
Then, the problem should be solved.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.