2025-10-21 5:33 AM
Hello,
I'm using STM32G474QET6 with HSI (16Mhz).
When not using DMA - the UART is working.
With DMA I'm having 2 issues:
The 2nd issue is the main issue.
That is my UART init func:
LL_USART_InitTypeDef usart_init_struct;
USART1->CR1 &= ~USART_CR1_UE; // Disable USART 1.
// USART 1 clock enable.
LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_USART1);
usart_init_struct.BaudRate = 19200;
usart_init_struct.DataWidth = LL_USART_DATAWIDTH_8B;
usart_init_struct.HardwareFlowControl = LL_USART_HWCONTROL_NONE;
usart_init_struct.OverSampling = LL_USART_OVERSAMPLING_16;
usart_init_struct.Parity = LL_USART_PARITY_EVEN;
usart_init_struct.PrescalerValue = LL_USART_PRESCALER_DIV1;
usart_init_struct.StopBits = LL_USART_STOPBITS_1;
usart_init_struct.TransferDirection = LL_USART_DIRECTION_TX_RX;
LL_USART_Init(USART1, &usart_init_struct);
USART1->CR3 |= USART_CR3_OVRDIS; // Disable Overrun error.
// Config DMA1_Ch4 for USART1 Rx, & DMA1_Ch_5 for USART1 Tx.
DmaConfig();
NVIC_EnableIRQ(USART1_IRQn);
USART1->CR1 |= USART_CR1_UE; // Enable USART 1.
And that is DmaConfig():
void DmaConfig(void)
{
LL_DMA_InitTypeDef dma_init_struc;
// DMA 1 & DMAMUX clock enable.
LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_DMA1 | LL_AHB1_GRP1_PERIPH_DMAMUX1);
/************************************
* Configuration for USART 1 Tx DMA *
************************************/
dma_init_struc.Direction = LL_DMA_DIRECTION_MEMORY_TO_PERIPH;
dma_init_struc.Mode = LL_DMA_MODE_NORMAL;
dma_init_struc.NbData = 0;
dma_init_struc.PeriphRequest = LL_DMAMUX_REQ_USART1_TX;
dma_init_struc.Priority = LL_DMA_PRIORITY_MEDIUM;
// Source.
dma_init_struc.MemoryOrM2MDstAddress = 0;
dma_init_struc.MemoryOrM2MDstDataSize = LL_DMA_MDATAALIGN_BYTE;
dma_init_struc.MemoryOrM2MDstIncMode = LL_DMA_MEMORY_INCREMENT;
// Destination.
dma_init_struc.PeriphOrM2MSrcAddress = (uint32_t)&USART1->TDR;
dma_init_struc.PeriphOrM2MSrcDataSize = LL_DMA_PDATAALIGN_BYTE;
dma_init_struc.PeriphOrM2MSrcIncMode = LL_DMA_PERIPH_NOINCREMENT;
DMA1_Channel5->CCR &= ~DMA_CCR_EN; // DMA disable.
LL_DMA_Init(DMA1, LL_DMA_CHANNEL_5, &dma_init_struc);
/*
* Enable USART_Tx DMA Transmit request.
* Enable DMA transmit complete interrupt.
* Clear DMA1 Ch5 ALL interrupt flags.
*/
USART1->CR3 |= USART_CR3_DMAT;
DMA1_Channel5->CCR |= DMA_CCR_TCIE;
DMA1->IFCR = DMA_IFCR_CGIF5;
NVIC_EnableIRQ(DMA1_Channel5_IRQn);
/************************************
* Configuration for USART 1 Rx DMA *
************************************/
dma_init_struc.Direction = LL_DMA_DIRECTION_PERIPH_TO_MEMORY;
dma_init_struc.Mode = LL_DMA_MODE_NORMAL;
dma_init_struc.NbData = 3;
dma_init_struc.PeriphRequest = LL_DMAMUX_REQ_USART1_RX;
dma_init_struc.Priority = LL_DMA_PRIORITY_MEDIUM;
// Source.
dma_init_struc.PeriphOrM2MSrcAddress = (uint32_t)&USART1->RDR;
dma_init_struc.PeriphOrM2MSrcDataSize = LL_DMA_PDATAALIGN_BYTE;
dma_init_struc.PeriphOrM2MSrcIncMode = LL_DMA_PERIPH_NOINCREMENT;
// Destination.
dma_init_struc.MemoryOrM2MDstAddress = (uint32_t)&data.bytes[1];
dma_init_struc.MemoryOrM2MDstDataSize = LL_DMA_MDATAALIGN_BYTE;
dma_init_struc.MemoryOrM2MDstIncMode = LL_DMA_MEMORY_INCREMENT;
DMA1_Channel1->CCR &= ~DMA_CCR_EN; // DMA disable.
LL_DMA_Init(DMA1, LL_DMA_CHANNEL_4, &dma_init_struc);
/*
* Enable USART_Rx DMA Receiver request.
* Enable DMA transmit complete interrupt.
* Clear DMA1 Ch4 ALL interrupt flags.
*/
USART1->CR3 |= USART_CR3_DMAR;
DMA1_Channel4->CCR |= DMA_CCR_TCIE;
DMA1->IFCR = DMA_IFCR_CGIF4;
//
NVIC_EnableIRQ(DMA1_Channel4_IRQn);
DMA1_Channel4->CCR |= DMA_CCR_EN; // DMA enable.
}
Solved! Go to Solution.
2025-10-24 2:54 AM
Yep, completely understood, and yet we all expect that the parity will be added by "itself".
Nice website, thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.