2021-11-10 6:56 AM
Hello !
I am currently working with a STM32F407VGT7 and I have troubles uploading some code in it. I did the simplest possible code with STM32CubeIDE : RCC configuration and some dummy operations in main while loop.
My problem is that after uploading code (with debug feature), starting it and pausing it a little while after (like 3 seconds or so), I got this error :
"Break at address "0x1fff36aa" with no debug information available, or outside of program code."
I have no idea what is causing this error. But seeing from STM32F407 datasheet that 0x1fff36aa is mapped in "System Memory + OPT" area, I guess this is not good...
I noticed that this bug doesn't occur if interrupts are disabled. Please find my code bellow.
Any idea of what could be causing this issue and how I could solve it ?
Thanks.
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
/* USER CODE BEGIN 2 */
uint32_t u32_dummy = 0;
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
// __disable_irq();
while (1)
{
/* USER CODE END WHILE */
u32_dummy += 24 * 56;
u32_dummy -= 12;
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
{
Error_Handler();
}
}
Solved! Go to Solution.
2021-11-10 7:03 AM
I found the issue : BOOT 0 pin is supposed to be pulled down (while it was pulled up).
2021-11-10 7:03 AM
I found the issue : BOOT 0 pin is supposed to be pulled down (while it was pulled up).
2021-11-10 8:59 AM
Hello @ERena.1 and welcome to the Community :)
Glad to know you overcame this problem, and thank you for your update.
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.