2020-05-06 2:26 AM
勾选了设置中的输入输出浮点,�?然无效。修改为标准库或者精简库也无效。网上也有很多人�?�到了这样的问题。请问怎么解决?官方有解决方案�?�?官方是�?�会在�?�期的版本中解决掉这个问题?
2020-05-10 2:53 PM
Hello,
Please ask your question in English.
Best Regards,
Imen
2020-05-10 10:31 PM
Stm32f4 uses stm32code ide to output floating-point numbers, and the program will enter a hardware error.
Setting the input and output floating-point options is also invalid. Changing to a standard or thin library is also not valid. There are also many people on the Internet who have encountered such problems. How can I solve it? Is there an official solution? Will the official fix the problem in a later version?
2020-05-10 10:33 PM
Maybe you want to read this thread:
https://community.st.com/s/question/0D50X0000Anrcyj/how-to-use-float-in-printf
JW
2020-05-13 12:55 AM
All methods have tried or can't print floating-point numbers
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.