STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! installation of the stm32cubeide

i have got a problem when i download stm32cubeide and install. i have download the file "en.gnu-tools-for-stm32-7-2018-q2-update.20190328-1800.zip" is correct? i have extracted the file, but can not find out the installation file in extract folder. ...

kevin xu by Associate II
  • 2185 Views
  • 3 replies
  • 0 kudos

Wrong download link for STM32CubeIDE

Tried downloading STM32CubeIDE for macOS and Linux (Debian installer). Both of these are not giving the correct download file. It seems to be some kind of source code package to compile a toolchain. Please help!

Include files not added to new source folder.

I created a new source folder in my file stucture, so I have the usual Core and Drivers folders, plus the FreeRTOS folder added by CubeIDE, then I have my App folder. See below.When I compile this, it compiles the three folders the IDE created, but f...

JMill.1 by Associate III
  • 1050 Views
  • 1 replies
  • 1 kudos

Build error VFP register argument (STM32F303RE nucleo board)

Hi, I'm trying to use the console in CubeIDE with my STM32F303RE nucleo board and use printf(). For this, I chose an empty project, not STMCube. In the tool settings, I set floating-point unit to none and Floating-point ABI to Software implementation...

JamB by Associate
  • 956 Views
  • 0 replies
  • 0 kudos

Debugging an STM32L152RE with Sleep causes exception in Code, but , running code after removing the emulator and power cycling functions correctly

I have a strange problem, I have ported the MBED-OS blinkly program to the IDE (this was a relatively painless process) , which sends the device to sleep between flashes. When I download and run the program with the emulator (I have tried blink, sti...

DFill.1 by Associate II
  • 2459 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.