2025-04-05 11:28 AM
Hey everyone :waving_hand:,
After installing STM32CubeIDE, I encountered the following warning:
"This peripheral has no parameter to be configured"
At first, I thought it was an error — but after doing some research, I realized it's probably nothing serious.
However, to be sure, I tried everything I could:
Reinstalled STM32CubeIDE
Changed system settings
Updated all available packages and tools
Despite all of this, the warning still appears whenever I configure certain peripherals.
Can someone help me understand if this is normal behavior? Should I ignore it, or is there a proper way to fix or suppress this warning?
Any guidance would be greatly appreciated!
Thanks in advance!
Solved! Go to Solution.
2025-04-05 12:04 PM
Hello @yashvee and welcome to the ST Community.
if you are tooking about the working in this Screenshot :
It is just added to mention that for this peripheral, there is not more parameter to be configured on the configuration window of the interface. For example, on the configuration of the USART, you will have some parameters to configure on the configuration menu.
Nothing to worry about.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-04-05 12:04 PM
Hello @yashvee and welcome to the ST Community.
if you are tooking about the working in this Screenshot :
It is just added to mention that for this peripheral, there is not more parameter to be configured on the configuration window of the interface. For example, on the configuration of the USART, you will have some parameters to configure on the configuration menu.
Nothing to worry about.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.