2024-05-16 1:16 AM - edited 2024-05-16 1:35 AM
Hello everyone,
I've just updated cubeIDE from V1.14.x to V1.15.1 and duration of build process on the same project increased by around 4x.
With V1.14 it took around ~10s, now with V1.15.1 takes ~40s to build the same project on the same machine.
Is that a known issue? How can I mitigate that?
Thank for your help!
BR, Žiga
2024-06-06 7:18 AM
Hello @zmiga
Could you provide your project in order to investigate the issue.
BR
Souhaib
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-06-27 10:39 PM - edited 2024-06-27 10:39 PM
Hi Souhaib,
unfortunatelly not, because it contains propriatery code.
What do you recommend for me? Should I downgrade to V1.14 version?
Are there any general tricks to speed up the build process?
Thank you!
BR, Žiga
2024-06-27 11:31 PM
I've downgraded to V1.14.1 and it compiles in less than 10 sec. Seems to be some specific problem with my PC setup and Cube V1.15 :thinking_face:
Additional info about the PC I'm using:
OS Version: 10.0.19045 N/A Build 19045
OS Manufacturer: Microsoft Corporation
OS Configuration: Member Workstation
System Manufacturer: Dell Inc.
System Model: OptiPlex 5060
System Type: x64-based PC
Processor(s): 1 Processor(s) Installed.
[01]: Intel64 Family 6 Model 158 Stepping 10 GenuineIntel ~3192 Mhz
BIOS Version: Dell Inc. 1.29.0, 29. 02. 2024
BR, Žiga
2024-09-16 1:10 AM
It gets worse on STM32CubeIDE Version: 1.16.0. What took ~10sec on V1.14.1 to compile the complete project, now on V1.16.0 takes 1m 28sec. That is over 8x longer.
I'll prepare some mockup application that I can share with you in order to get to the bottom of that problem.
In the meanwhile, can you point out some thing to check? Did you maybe take some time to investigate?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.