2019-12-14 11:22 PM
Hello!
Then i've upgraded STM32CubeIDE v. 1.0.2 for macOS to v. 1.1.0, i can't load program to my Nucleo L476RG board. With v. 1.0.2 all works fine.
Error: Data mismatch found at address 0x08000004 (byte = 0x75 instead of 0xA9).
i tried to remove "Verify flash download" flag on Debug settings. After that, board becomes broken. Error: Device not found.
P.S. Then i directly download v.1.1.0 .dmg file (not using "Check for updates") i get "Program corrupted - move to Trash" error after installation.
Full log:
STMicroelectronics ST-LINK GDB server. Version 5.3.2
Copyright (c) 2019, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 31
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Enabled
SWD Debug : Enabled
Target connection mode: Attach
Hardware watchpoint supported by the target
COM frequency = 4000 kHz
ST-LINK Firmware version : V2J34M25
Device ID: 0x415
PC: 0x8009dbc
ST-LINK device status: HALT_MODE
ST-LINK detects target voltage = 3.27 V
ST-LINK device status: HALT_MODE
ST-LINK device initialization OK
Waiting for debugger connection...
Waiting for connection on port 61234...
Accepted connection on port 61234...
Debugger connected
Enter STM32_AppReset() function
NVIC_DFSR_REG = 0x00000009
NVIC_CFGFSR_REG = 0x00000000
XPSR = 0x01000000
------ Switching to STM32CubeProgrammer -----
[36m[01m -------------------------------------------------------------------
[39;49m[36m[01m STM32CubeProgrammer v2.2.0
[39;49m[36m[01m -------------------------------------------------------------------
[39;49m[39;49m
[39;49m[39;49mLog output file: /tmp/STM32CubeProgrammer_STfVay.log
[39;49m[39;49m[39;49m[39;49m[90mST-LINK SN : 066CFF575255878281031937
[39;49m[90mST-LINK FW : V2J34M25
[39;49m[90mVoltage : 3.26V
[39;49m[90mSWD freq : 4000 KHz
[39;49m[90mConnect mode: Under Reset
[39;49m[90mReset mode : Hardware reset
[39;49m[90mCannot identify the device
[39;49m[00;31mError: unknown or unsupported device (DevID = 0x0000)
[39;49m[39;49m
[39;49m[39;49mMemory Programming ...
[39;49m[39;49mOpening and parsing file: ST-LINK_GDB_server_PjlniY.srec
[39;49m[39;49m File : ST-LINK_GDB_server_PjlniY.srec
[39;49m[39;49m Size : 56384 Bytes
[39;49m[39;49m Address : 0x08000000
[39;49m[39;49m
[39;49m[39;49m[39;49mErasing memory corresponding to segment 0:
[39;49m[39;49m[39;49mDownload in Progress:
[39;49m[39;49m[39;49m[39;49m[39;49m[39;49m[00;32m[==================================================] 100%
[39;49m[39;49m[39;49m
[39;49m[00;32mFile download complete
[39;49m[39;49mTime elapsed during download operation: 00:00:00.427
[39;49m[39;49m
[39;49m[39;49m
Verifying ...
[39;49m[39;49m
[39;49m[39;49mRead progress:
[39;49m[39;49m[39;49m[00;32m[= ] 3%
[39;49m[39;49m
[39;49mError: Data mismatch found at address 0x08000004 (byte = 0x75 instead of 0xA9)
[39;49m[39;49m
[39;49m[00;31mError: Download verification failed
[39;49m[39;49m
[39;49mEncountered Error when opening /Applications/STM32CubeIDE.app/Contents/Eclipse/plugins/com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.macos64_1.1.0.201910081157/tools/bin/STM32_Programmer_CLI
------ Switching context -----
Error in STM32CubeProgrammer
Debugger connection lost.
Shutting down...
2020-01-10 12:58 AM
Sounds STM32CubeIDE 1.2.0 release should solve issue ! which was apparently "only" a macOS support issue
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.