2019-06-19 5:14 PM
If I double click on the supposedly missing include file CubeIDE finds the file in the project path just fine...
I seem to have to recreate the project in MX / clean-re-build to get the libraries to re-figure out that they exist. Very strange.
Is there another non-buggy compiler that I should use that integrates with Cube ? Im on the Stm32L4 so I think I need to pay for the Keil IDE.
2019-06-25 1:40 AM
Do you do anything in particular once the files "go missing"? Is it with a fresh launch of CubeIDE or something like that?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.