2024-03-12 2:07 AM
Hello,
i need help how to edit linker file for placing array on specific address in external SDRAM connected via FMC.
I'm working with 7" TFT 800x480 @ 24bpp via LTDC controller and i have configuration 2 layers and both double buffered. So in HW is connected external SDRAM 8MB four banks (2MBx4). I would like to use each bank for one buffer as recommended in AN4861 https://www.st.com/resource/en/application_note/an4861-lcdtft-display-controller-ltdc-on-stm32-mcus-stmicroelectronics.pdf.
I added SDRAM and SDRAM section into linker script as follows:
SDRAM (rwx) : ORIGIN = 0xC0000000, LENGTH = 8192K
...
...
.sdram (NOLOAD) :
{
. = ALIGN(4);
*(.sdram .sdram.*)
} > SDRAM
But i don't know how to place four buffers into start address of each SDRAM bank.
I tried to create 4 SDRAM sections instead of one:
SDRAM0 (rwx) : ORIGIN = 0xC0000000, LENGTH = 2048K
SDRAM1 (rwx) : ORIGIN = 0xC0200000, LENGTH = 2048K
SDRAM2 (rwx) : ORIGIN = 0xC0400000, LENGTH = 2048K
SDRAM3 (rwx) : ORIGIN = 0xC0600000, LENGTH = 2048K
...
...
/* external SDRAM0 */
.sdram0 (NOLOAD) :
{
. = ALIGN(4);
*(.sdram0 .sdram0.*)
} > SDRAM0
/* external SDRAM1 */
.sdram1 (NOLOAD) :
{
. = ALIGN(4);
*(.sdram1 .sdram1.*)
} > SDRAM1
/* external SDRAM2 */
.sdram2 (NOLOAD) :
{
. = ALIGN(4);
*(.sdram2 .sdram2.*)
} > SDRAM2
/* external SDRAM3 */
.sdram3 (NOLOAD) :
{
. = ALIGN(4);
*(.sdram3 .sdram3.*)
} > SDRAM3
and declare variables as:
uint32_t lcd_buffer0[288000] __attribute__((section(".sdram0")));
uint32_t lcd_buffer1[288000] __attribute__((section(".sdram1")));
uint32_t lcd_buffer2[288000] __attribute__((section(".sdram2")));
uint32_t lcd_buffer3[288000] __attribute__((section(".sdram3")));
But i don't know if it's correct approach.
Can you help me how to do it?
Solved! Go to Solution.
2024-03-12 6:17 AM
That is the correct approach. Does it compile and work? Might be missing some subtle syntax but the idea is correct.
2024-03-12 6:17 AM
That is the correct approach. Does it compile and work? Might be missing some subtle syntax but the idea is correct.
2024-03-12 6:46 AM
@Petr3 You don't even need to touch the link script. Just define the addresses as standard C pointers with absolute values. For example
#define lcd_buffer0 ((uint8_t*)0xC0000000)
....
#define lcd_buffer3 ((uint8_t*)0xC0600000)
2024-03-12 9:33 AM
Yes, it seems to work fine. List file shows, that buffers are placed on correct adddres in external SDRAM.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.