2024-05-09 8:12 PM
11:06:38 **** Incremental Build of configuration Debug for project STM32H747I-DISCO_CM7 ****
make all
arm-none-eabi-arm-none-eabi-arm-none-eabi-gcc -o "STM32H747I-DISCO_CM7.elf" @"objects.list" -l:libtouchgfx-float-abi-hard.a -mcpu=cortex-m7 -T"G:\TouchGFX\TouchGFXProjects\MyDemo\STM32CubeIDE\CM7\STM32H747XIHX_FLASH.ld" --specs=nosys.specs -Wl,-Map="STM32H747I-DISCO_CM7.map" -Wl,--gc-sections -static -L../../../CM7/Middlewares/ST/touchgfx/lib/core/cortex_m7/gcc --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -Wl,--start-group -lc -lm -lstdc++ -lsupc++ -Wl,--end-group
g:/stm32cubeide_1.15.1/stm32cubeide/plugins/com.st.stm32cube.ide.mcu.externaltools.make.win32_2.1.300.202402091052/tools/bin/sh: arm-none-eabi-arm-none-eabi-arm-none-eabi-gcc: not found
make: *** [makefile:103: STM32H747I-DISCO_CM7.elf] Error 127
"make all" terminated with exit code 2. Build might be incomplete.
11:06:40 Build Failed. 1 errors, 0 warnings. (took 2s.517ms)
How to solve this problem?
2024-05-10 3:43 PM - edited 2024-05-10 3:45 PM
> arm-none-eabi-arm-none-eabi-arm-none-eabi-gcc: not found
The ARM toolchain is not found. Check in the project properties that the toolchain is installed. If not - either install the needed toolchain or select one of available toolchains.
2024-05-13 8:19 PM
thanks,I solved the problem by regenerating the code with touchgfx, then configuring it with cubeMX, and then recompiling it in cubeIDE.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.