2023-03-10 9:12 AM
I have been having this issue reoccuring and has only started in the past month. I have upgrade and downgraded versions (currently back at 1.12.0) with hopes to fix it and while it goes away for a bit and I am able to work with the live debugging for a bit it always returns.
The two behaviours are giving me an error with the register 0 or the following:
"Board : STLINK-V3SET
Voltage : 3.28V
SWD freq : 8000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x450
Revision ID : Rev V
Device name : STM32H7xx
Flash size : 2 MBytes
Device type : MCU
Device CPU : Cortex-M7
BL Version : 0x90
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a07300.srec
File : ST-LINK_GDB_server_a07300.srec
Size : 110.96 KB
Address : 0x08020000
Erasing memory corresponding to segment 0:
Erasing internal memory sector 1
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:01.236
Verifying ...
Download verified successfully
Shutting down...
Exit."
I usually can get this issue to go away after playing around with the Debug Configurations, but so far nothing reproducible.
2023-03-13 4:03 AM
Hello @RMack.1 ,
At first, let me thank you for reporting this issue.
Are you using the right debug buttom and not the run buttom. Because, everything is downloaded successfully.
Thanks,
Rim
2023-03-15 10:53 AM
Yes I am sure I am selecting the "Debug"
So far I am able to resolve this issue by comparing the ".launch" files for a previously working file but I am still not sure why it would be changing this file's settings. The alternative error it has been getting is:
"Failed to assign value 80224ed, to register 0
Failed to assign value 240375f8, to register 0
Failed to assign value 2407fff8, to register 0
Failed to assign value 803f332, to register 0"
It seems to happen after a crash of the IDE but still seems to be altering the launch settings for the debugging.
2023-03-16 3:57 AM
Hello @RMack.1 ,
Could you, please, provide :
It would be, also, helpful to provide the whole projects you are working on .
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.