2024-04-22 12:14 PM
I am using nucleo-f439zi in stm32cubeide with freertos debug. It seems everything is working, the only thing is that I need pause program if I would like to see freertos task list status. Is it possible to track task list status when system is running?
2024-04-23 8:20 AM
Hello @yang hong,
In stm32CubeIDE, the following views are available for FreeRTOS:
If the Run Time column in the FreeRTOS Task List view displays after making three settings
Please check the settings in paragraph 3.4.2.1.3 RTOS profiling information in UM2609
PS: the problem can arise if project is not built with an optimization level -O0
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-04-23 10:00 AM
I did all following manual instruction for FreeRTos, however, I still need suspend program to make FreeRTOS task list update. Is it true for this feature?
2024-04-23 10:59 AM
Ok,
Finally, I got some explanation from manual.
Frankly, I am little bit disappointed because stm32cubeide can't make task list view to update during the program running.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.