2020-02-21 8:10 AM
Hi,
I wanted to start learning FreeRTOS. I'm working with a L082 device, using CubeIDE. In the config file, I only can select CMSIS-RTOS v1 interface, v2 is disabled. But there's no explanation why.
So, I don't know if the device is unsupported by v2 or if there's something missing. I assume I can get it to work with v1, but...
Regards
Solved! Go to Solution.
2020-02-23 7:53 AM
> So, I don't know if the device is unsupported by v2 or if there's something missing. I assume I can get it to work with v1, but...
When you hoover the mouse over CMSIS_V2 is lists the supported series. L0 is not among them.
2020-02-23 7:53 AM
> So, I don't know if the device is unsupported by v2 or if there's something missing. I assume I can get it to work with v1, but...
When you hoover the mouse over CMSIS_V2 is lists the supported series. L0 is not among them.
2020-02-23 10:51 PM
Ah, okay. Thank you. Sometimes it's not clear if an option is disabled because of missing settings or because the device doesn't support it. Now it's clear.
Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.