2022-05-28 10:52 AM
I working with the stm32cubeide version 1.9.0, stlink-v3 debugger and the stm32l4r9 with 1M flash. Everything was going fine until the code size reached 128 sectors ( ~ 50% of the flash). I'm now getting the following error when I attempt to download and debug the application:
STMicroelectronics ST-LINK GDB server. Version 6.1.0
Copyright (c) 2022, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
-------------------------------------------------------------------
STM32CubeProgrammer v2.10.0
-------------------------------------------------------------------
Log output file: /tmp/STM32CubeProgrammer_ZLtEAK.log
ST-LINK SN : 005500333137511533333639
ST-LINK FW : V3J9M3B5S1
Board : STLINK-V3SET
Voltage : 3.35V
JTAG freq : 21333 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x470
Revision ID : Rev W
Device name : STM32L4Rxxx/STM32L4Sxxx
Flash size : 1 MBytes
Device type : MCU
Device CPU : Cortex-M4
BL Version : --
Debug in Low Power mode enabled
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_GjIRXM.srec
File : ST-LINK_GDB_server_GjIRXM.srec
Size : 512.24 KB
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 128]
Download in Progress:
Error: failed to download Segment[0]
Error: failed to download the File
Note: If I reduce the code size to 126 sectors or less, then I can download debug as expected.
Any ideas
Solved! Go to Solution.
2022-05-30 1:34 PM
It appears I have found a permanent solution for the "failed to download Segment[0] when code size reaches 50% of flash" issue. The solution for me was to uncheck the DB1M ( Changing dual flash bank mode to single flash bank mode) within the STM32Programmer's user configuration settings and update the chip.
2022-05-28 1:02 PM
For the benefit of others, I'm answering my own questions. Keep in mind this is my first time using any ST parts.
I suspected the issue was related to the flash protection bits but was unable to find a way within the STM32CubeIDE to address the issue. After posting this question and further research, I discovered that ST has a standalone Programmer utility. This utility can be used to correct the issue. Download and install the standalone stm32programmer utility. Run the utility, select the "OB" tab, then select Read out protection. Ensure it is set to AA, then go to the Erase and Programming Tab, click full chip erase. After that you should be able to continue as normal.
Not sure how to mark this as SOLVED
2022-05-28 2:15 PM
>>Not sure how to mark this as SOLVED
Select as "best answer"
2022-05-28 7:28 PM
So it appears my solution is only temporary. After downloading and debugging a few times the issue returns. I can repeat the process of using the standalone programmer to erase the flash and once again it will work. I don't understand why this is happening. Anyone want to take a stab at it.
This is an in-house developed board, so I'm fully responsible for the design and can change it. But this is rather simple setup 3 spi interfaces and 2 i2c interface and a CAN bus interface.
The code size is is mostly due to using lvgl library on a spi display with touch screen. I haven't attempted to optimise this library yet so it's a little big, I'm not attempting to use any of the protection mechanisms in the processor. I have physical hardware reset attached to the jtag interface. However I have notice that I often have to download and debug the code a second time in-order to get it to properly run and debug. It would appear the processor is not properly resetting I've tried hardware reset, connect under reset etc. none of this appear to have any effect.
2022-05-30 1:34 PM
It appears I have found a permanent solution for the "failed to download Segment[0] when code size reaches 50% of flash" issue. The solution for me was to uncheck the DB1M ( Changing dual flash bank mode to single flash bank mode) within the STM32Programmer's user configuration settings and update the chip.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.