2023-09-14
7:26 PM
- last edited on
2023-09-15
6:05 AM
by
Lina_DABASINSKA
Hi
I m working on NUCLEO-H723 Board, was programming SPI and is working fine, when trying to add USART function to display text on serial terminal and encountered the following errors, unable to make sense what went wrong, anyone can help ? thx.
arm-none-eabi-gcc "../Core/Src/gpio.c" -mcpu=cortex-m7 -std=gnu11 -g3 -DDEBUG -DUSE_HAL_DRIVER -DSTM32H723xx -c -I../Core/Inc -I../Drivers/STM32H7xx_HAL_Driver/Inc -I../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Core/Src/gpio.d" -MT"Core/Src/gpio.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Core/Src/gpio.o"
arm-none-eabi-gcc "../Core/Src/main.c" -mcpu=cortex-m7 -std=gnu11 -g3 -DDEBUG -DUSE_HAL_DRIVER -DSTM32H723xx -c -I../Core/Inc -I../Drivers/STM32H7xx_HAL_Driver/Inc -I../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Core/Src/main.d" -MT"Core/Src/main.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Core/Src/main.o"
arm-none-eabi-gcc -o "SPI_PWRSTP01_USART.elf" @"objects.list" -mcpu=cortex-m7 -T"C:\Users\goh\STM32CubeIDE\workspace_1.13.1\proj_USART-v1\proj_USART\STM32H723ZGTX_FLASH.ld" --specs=nosys.specs -Wl,-Map="proj_USART.map" -Wl,--gc-sections -static --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -Wl,--start-group -lc -lm -Wl,--end-group
C:/ST/STM32CubeIDE_1.13.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.0.202305231506/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: ./Core/Src/usart.o:C:/Users/goh/STM32CubeIDE/workspace_1.13.1/SPI_PWRSTP01_USART-v1/SPI_PWRSTP01/Debug/../Core/Src/usart.c:27: multiple definition of `huart3'; ./Core/Src/main.o:C:/Users/goh/STM32CubeIDE/workspace_1.13.1/SPI_PWRSTP01_USART-v1/SPI_PWRSTP01/Debug/../Core/Src/main.c:53: first defined here
collect2.exe: error: ld returned 1 exit status
2023-09-14 8:33 PM
I would say you're posting in the wrong forum, but there's actually no description anywhere on what the "Feedback Forum" is for.
Historically, the feedback forum is not meant for technical questions.
2023-09-14 8:42 PM
>> multiple definition of `huart3';
So DON'T do that. Create the instance in one file, make extern references in others, and in include files, etc.
2023-09-15 6:03 AM
Hello @TDK ,
Well noted. The description is now in place!
Thanks,
Lina
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.