2023-12-13 12:17 PM
Hallo,
when i will generate code. The message in a message box is:
Error downloading the following files:
stm32cube_fw_IO_v1122.zip (Not available)
For unaavailable files, you can load them manually with the 'From Local' button.
My problem is i can't found the 'From Local' button oran alternative way to download the file.
Best regards
Solved! Go to Solution.
2023-12-18 10:21 AM
Hello colleagues,
many thanks for the support. In the meantime I was able to solve the problem. Two other computers on the same WiFi network were able to download the files. The problem lies with the computer. After I have ended some of the background processes, I can also download the files on the other computer!
Thanks for your support
2023-12-13 1:51 PM
Welcome @Bitman, to the community!
Which version of STM32CubeIDE are you using?
If it is the latest version: are you logged into the IDE with your credentials?
Regards
/Peter
2023-12-13 11:32 PM
Hello,
are you sure it is IO in the zip filename ? It looks like L0 in lowercase, huh... Normally the archive name contains the MCU series.
It could help to know which MCU is in your project.
2023-12-14 4:56 AM
2023-12-15 4:32 AM
You did not answer my question about the MCU, I guess you are using an MCU from L0 series...
Sorry I tried to reproduce but it works fine on my side. I can download the FW pack, install it and build a project using it.
Have you tried to refresh the FW pack data through menu Help > Embedded Software Package Manager > Refresh ?
2023-12-18 10:21 AM
Hello colleagues,
many thanks for the support. In the meantime I was able to solve the problem. Two other computers on the same WiFi network were able to download the files. The problem lies with the computer. After I have ended some of the background processes, I can also download the files on the other computer!
Thanks for your support
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.