2024-02-27 3:03 PM - edited 2024-02-28 9:31 AM
The bug which was introduced in 1.14.0 which prevents a post-build step command to run, still exists in 1.14.1 with my project.
I have a Windows batch file which should be run after build, and has worked correctly before version 1.14.0
The result of the build post step is:
..\postprocess.bat
make[1]: *** [makefile:97: post-build] Error -1
make: *** [makefile:65: all] Error 2
"make -j4 all" terminated with exit code 2. Build might be incomplete.
Resolution in following post.
2024-02-28 9:30 AM
It appears that the post-build command is now intolertant of spaces in project paths.
I was able to resolve the problem in my case by surrounding my batch file name in double-quotation marks as follows:
"..\postprocess.bat" param1 param2
2024-07-01 2:25 AM
Thank EdGi.
This also worked for me using STM32CubeIDE v1.15.1
2025-06-05 5:49 PM
Thank you so much for your post, it really helped me!
1.17.0
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.