cancel
Showing results for 
Search instead for 
Did you mean: 

stlink-server how to bind to all addreses inferfaces instead on local host?

PPavl.2
Associate
 
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
MM..1
Chief III

For example on my system in c:\ST\com.st.stm32cube.ide.mcu.externaltools.stlink-gdb-server.win32_1.6.0.202101291314\tools\bin\

i create config.txt and start persistent ST-LINK_gdbserver.bat , that i can connect from other world place over forwarded debug port...

PPavl.2
Associate

I can"t find the option for changing address:

root@Debug-0:~# /usr/bin/stlink-server --help

stlink-server

--help      | -h      display this help

--version   | -v      display STLinkserver version

--port      | -p      set tcp listening port

--debug     | -d      set debug level <0-5> (incremental, 0: Error, 1:Info, 2:Warning, 3:STlink,

4:Debug, 5:Usb)

--auto-exit | -a      exit() when there is no more client

--log-output | -l      redirect log output to file <name>

MM..1
Chief III

Seems on windows works ok, but for linux limited to localhost?

C:\Users\spravca>netstat -na
 
Active Connections
 
  Proto  Local Address          Foreign Address        State
  TCP    0.0.0.0:135            0.0.0.0:0              LISTENING
  TCP    0.0.0.0:445            0.0.0.0:0              LISTENING
  TCP    0.0.0.0:990            0.0.0.0:0              LISTENING
  TCP    0.0.0.0:2869           0.0.0.0:0              LISTENING
  TCP    0.0.0.0:5357           0.0.0.0:0              LISTENING
  TCP    0.0.0.0:49152          0.0.0.0:0              LISTENING
  TCP    0.0.0.0:49153          0.0.0.0:0              LISTENING
  TCP    0.0.0.0:49154          0.0.0.0:0              LISTENING
  TCP    0.0.0.0:49157          0.0.0.0:0              LISTENING
  TCP    0.0.0.0:49158          0.0.0.0:0              LISTENING
  TCP    0.0.0.0:50128          0.0.0.0:0              LISTENING
  TCP    0.0.0.0:61234          0.0.0.0:0              LISTENING
STMicroelectronics ST-LINK GDB server. Version 5.8.0
Copyright (c) 2020, STMicroelectronics. All rights reserved.
 
Starting server with the following options:
        Persistent Mode            : Enabled
        LogFile Name               : debug.log
        Logging Level              : 31
        Listen Port Number         : 61234
        Status Refresh Delay       : 15s
        Verbose Mode               : Disabled
        SWD Debug                  : Enabled
 
Target connection mode: Default
Reading ROM table for AP 0 @0xe00fffd0
Hardware watchpoint supported by the target
COM frequency = 4000 kHz
ST-LINK Firmware version : V2J37M26
Device ID: 0x421
PC: 0x8000e38
ST-LINK device status: HALT_MODE
ST-LINK detects target voltage = 3.25 V
ST-LINK device status: HALT_MODE
ST-LINK device initialization OK
Waiting for debugger connection...
Waiting for connection on port 61234...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.