STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32CubeIDE is damaged and corrupted, how to fix?

Hello,I am a high school student trying to do a project that requires the use of the STM32CubeIDE.My OS is macOS Mojave 10.14.5. I have a little under 10GB of space in free storage.I am able to download the file off the website, unzip it, and run the...

ZTu.1 by Associate
  • 1223 Views
  • 0 replies
  • 0 kudos

Resolved! What is the trick to view SFRs in debug?

My sincere apologies for what I am sure is an idiot newbie's error. Thank you everyone for your time.I have STM32CubeIDE and I do not seem to be able to read back values of SFRs (peripheral registers) while in debug. E.g. my code containsHRTIM1_MASTE...

VGusi.1 by Associate II
  • 3679 Views
  • 3 replies
  • 0 kudos

Resolved! STM32CubeIDE 1.7.0 code on STM32G0B1 CAN bus ID filter not working once using (HAL_FDCAN_ConfigGlobalFilter(&hfdcan1, FDCAN_REJECT, FDCAN_REJECT, FDCAN_FILTER_REMOTE, FDCAN_FILTER_REMOTE) .

Classic CAN configuration as below. when the line "if(HAL_FDCAN_ConfigGlobalFilter(...))" is removed, the CAN messages are received without issue. The transmitted message is set as ID: 0x111 . Confirmed by a CAN bus monitor.Configuration as below:FDC...

Jackle by Associate III
  • 4576 Views
  • 6 replies
  • 0 kudos

Thread safe malloc

I am currently writing a code on stm32l496vg with freertos. I came across a lot warnings about malloc thread safety issue. Now, cubeide 1.7.0 says it provides thread safe malloc in default. Is problem solved now?What is the exact release date of cube...

SAkta.1 by Associate
  • 1340 Views
  • 1 replies
  • 0 kudos

stm32cube ide and iar ide

I am using bno080 dev board with nucleo board.I have the code from github which is done in the IAR IDE.https://github.com/hcrest/bno080-nucleo-demo/I am using stm32cubeide....While initializing the project in IAR IDE they asked to enable i2c configur...

AR.7 by Associate II
  • 1064 Views
  • 0 replies
  • 0 kudos

Resolved! Excessive resource usage

Hi, I am attaching a simple .ioc configuration file with which I generated a new project using stm32 cubeide which when compiled generates a footprint of about 12kB.Frankly, it seems excessive to me, to the point of making this platform unusable for ...

I am trying to discover things about the IDE, but there is a problem. The IDE's information centre isn't working. Clicking on the blue I, information gives me the following error:

/...../workspace/.metadata/.plugins/com.st.stm32cube.ide.mcu.informationcenter/tech-doc.html: No such file or directory, on a linux OS. But I can find it manually! The file links in that document point to non existent directory in the path. The pat...

petereiso by Associate II
  • 3210 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.