cancel
Showing results for 
Search instead for 
Did you mean: 

SMCubeIDE Live Expressions - Incorrect Data Framing (Weird)

Garnett.Robert
Senior III

Hi,

 

I have a functioning project that fully compiles with only three warnings, but when I debug it and examine C structures in the live expressions viewer the the data (GovTrimControl_P structure ) appears to be offset by 4 bytes, yet the memory browser shows the correct values and when the mouse hovers over a value that value is correct:

 

Snag_190db9f0.png

 

Snag_190ed747.png

Snag_191550df.png

 

The Build Analyser also reports the address of GovTrimControl_P  correctly

Snag_1918f31c.png

Compile Problem Output:

Snag_1916f2f6.png

The values for the GovTrimControl_P structure are set at bootup to:

 

 

 

/* Parameters (default storage) */
struct P_GovTrimControl_T_
{
  real32_T FreqSP;                     /* Variable: FreqSP */                              
  real32_T kD;                         /* Variable: kD */
  real32_T kI;                         /* Variable: kI */                                       
  real32_T kN;                         /* Variable: kN */
  real32_T kP;                         /* Variable: kP */
};

typedef struct P_GovTrimControl_T_ P_GovTrimControl_T;

/* Block parameters (default storage) */
P_GovTrimControl_T GovTrimControl_P =
{
  /* Variable: FreqSP */
  50.0F,

  /* Variable: kD */
  2.0F,

  /* Variable: kI */
  20.0F,

  /* Variable: kN */
  2.0F,

  /* Variable: kP */
  30.0F
};

 

 

The problem also occurs with another constant array where the Live Expression viewer reports incorrect framing of the underlying data.

I am running STM32CubeIDE Version

Version: 1.16.1

Build: 22882_20240916_0822 (UTC)

 

On an STM32H750B-DK Discovery kit,

 

I have attached the Linker Script File, startup file and video in the hope this might shed some light on the issue. The video shows the Backup ram memory which has the GovTrimControl_P data copied into it. The data shows the correct framing in the browser, but not in the Live Expression viewer:

 

Snag_192b6556.png

 The backup ram copy function and its use are shown below:

 

 

 

void backupRamStartup(uint16_t bypassBtnState,
uint32_t code,									uint32_t* ramCode,
void* ramAddr,
void* parameters,
uint16_t size)
{
	if((bypassBtnState == 1) || (*ramCode != code))
	{
		/* The user is setting the defaults or the backupRam is empty */
		*ramCode = code;
		memcpy(ramAddr, parameters, size);
		return;
	}
	/* The backup ram contents are used to set the parameters*/
	memcpy(&parameters, &ramAddr, size);
}

/* Useage */

backupRamStartup(  								        HAL_GPIO_ReadPin(PC13_PB_DEFAULT_SET_GPIO_Port, 
PC13_PB_DEFAULT_SET_Pin),
0xC0AD1234,
&backupRAMValidationCode,
&backupRam,
&GovTrimControl_P,
sizeof(GovTrimControl_P));

 

 

 

I have never seen this occur in any of my other similar projects with older versions of the IDE.

 

Has anyone else seen this problem

 

Kind Regards

Rob

 

 

 

 

/* LINKER SCRIPT */
/* Entry Point */
ENTRY(Reset_Handler)

/* Highest address of the user mode stack */
_estack = ORIGIN(RAM_D1) + LENGTH(RAM_D1);	/* end of "RAM_D1" Ram type memory */

_Min_Heap_Size = 0x1000;	/* required amount of heap  */
_Min_Stack_Size = 0x1000;	/* required amount of stack */

/* Memories definition */
MEMORY
{
  DTCM_STACK    	(xrw)   : ORIGIN = 0x20000000,   		LENGTH = _Min_Heap_Size + _Min_Stack_Size
  DTCM_MISC	   		(xrw)    : ORIGIN = 0x20002000,   		LENGTH = 120K
  ITCMRAM      		(xrw)    : ORIGIN = 0x00000000,   		LENGTH = 64K
  RAM_D1       		(xrw)    : ORIGIN = 0x24000000,   		LENGTH = 512K
  RAM_D2       		(xrw)    : ORIGIN = 0x30000000,   		LENGTH = 288K
  RAM_D3       		(xrw)    : ORIGIN = 0x38000000,   		LENGTH = 64K
  SDRAM_FB     		(xrw)    : ORIGIN = 0xD0000000,   		LENGTH = 765K
  SDRAM_USER   		(xrw)    : ORIGIN = 0xD0000000 + 765K,  LENGTH = 8M - 765K
  FLASH	       		(xr)     : ORIGIN = 0x90000000,   		LENGTH = 2048K
  ASSETS_FLASH 		(r)      : ORIGIN = 0x90200000,   		LENGTH = 126M
  BOOTLOADER   		(xrw)    : ORIGIN = 0x08000000,   		LENGTH = 128k
  VBAT_SRAM_CODE	(xrw)    : ORIGIN = 0x38800000,  		LENGTH = 4
  VBAT_SRAM	   		(xrw)    : ORIGIN = 0x38800000 + 4,   	LENGTH = 4K - 4
}

TARGET(binary) /* specify the file format of binary file */
INPUT (../../ExtMem_Boot/bootloader.bin) /* bootloader bin file path (relative to the output folder)*/
OUTPUT_FORMAT(default) /* restore the out file format */

/* Sections */
SECTIONS
{
  .bootloader :
  {
    . = ALIGN(4);
    KEEP(../../ExtMem_Boot/bootloader.bin)
  } > BOOTLOADER

  /* The startup code into "FLASH" Rom type memory */
  .isr_vector :
  {
    __ICFEDIT_intvec_start__ = .;
    . = ALIGN(4);
    KEEP(*(.isr_vector)) /* Startup code */
    . = ALIGN(4);
  } >FLASH

  /* The program code and other data into "FLASH" Rom type memory */
  .text :
  {
    . = ALIGN(4);
    *(.text)           /* .text sections (code) */
    *(.text*)          /* .text* sections (code) */
    *(.glue_7)         /* glue arm to thumb code */
    *(.glue_7t)        /* glue thumb to arm code */
    *(.eh_frame)

    KEEP (*(.init))
    KEEP (*(.fini))

    . = ALIGN(4);
    _etext = .;        /* define a global symbols at end of code */
  } >FLASH

  /* Constant data into "FLASH" Rom type memory */
  .rodata :
  {
    . = ALIGN(4);
    *(.rodata)         /* .rodata sections (constants, strings, etc.) */
    *(.rodata*)        /* .rodata* sections (constants, strings, etc.) */
    . = ALIGN(4);
  } >FLASH

  .ARM.extab (READONLY) : {
    . = ALIGN(4);
    *(.ARM.extab* .gnu.linkonce.armextab.*)
    . = ALIGN(4);
  } >FLASH

  .ARM (READONLY) :  {
    . = ALIGN(4);
    __exidx_start = .;
    *(.ARM.exidx*)
    __exidx_end = .;
    . = ALIGN(4);
  } >FLASH

  .preinit_array  (READONLY)   :
  {
    . = ALIGN(4);
    PROVIDE_HIDDEN (__preinit_array_start = .);
    KEEP (*(.preinit_array*))
    PROVIDE_HIDDEN (__preinit_array_end = .);
    . = ALIGN(4);
  } >FLASH

  .init_array (READONLY) :
  {
    . = ALIGN(4);
    PROVIDE_HIDDEN (__init_array_start = .);
    KEEP (*(SORT(.init_array.*)))
    KEEP (*(.init_array*))
    PROVIDE_HIDDEN (__init_array_end = .);
    . = ALIGN(4);
  } >FLASH

  .fini_array (READONLY) :
  {
    . = ALIGN(4);
    PROVIDE_HIDDEN (__fini_array_start = .);
    KEEP (*(SORT(.fini_array.*)))
    KEEP (*(.fini_array*))
    PROVIDE_HIDDEN (__fini_array_end = .);
    . = ALIGN(4);
  } >FLASH

  /* Used by the startup to initialize data */
  _sidata = LOADADDR(.data);

  /* Initialized data sections into "RAM_D1" Ram type memory */
  .data :
  {
    . = ALIGN(4);
    _sdata = .;        /* create a global symbol at data start */
    *(.data)           /* .data sections */
    *(.data*)          /* .data* sections */

    . = ALIGN(4);
    _edata = .;        /* define a global symbol at data end */

  } >RAM_D1 AT> FLASH

  /* Uninitialized data section into "RAM_D1" Ram type memory */
  . = ALIGN(4);
  .bss :
  {
    /* This is used by the startup in order to initialize the .bss section */
    _sbss = .;         /* define a global symbol at bss start */
    __bss_start__ = _sbss;
    *(.bss)
    *(.bss*)
    *(COMMON)

    . = ALIGN(4);
    _ebss = .;         /* define a global symbol at bss end */
    __bss_end__ = _ebss;
  } >RAM_D1

  /* User_heap_stack section, used to check that there is enough "RAM_D1" Ram  type memory left */
  ._user_heap_stack :
  {
    . = ALIGN(8);
    PROVIDE ( end = . );
    PROVIDE ( _end = . );
    . = . + _Min_Heap_Size;
    . = . + _Min_Stack_Size;
    . = ALIGN(8);
  } >DTCM_STACK


  .DTCM_MISC : {
  . = ALIGN(4);
  _sDTCM_MISC = .;
  __sDTCM_MISC__ = _sDTCM_MISC;
  *(.DTCM_MISC) /* All nominated variables */
  	. = ALIGN(4);
  _eDTCM_MISC = .;
  __eDTCM_MISC__ = _eDTCM_MISC;
  } >DTCM_MISC


  .VBAT_SRAM_CODE (NOLOAD) :  {
  . = ALIGN(4);
  _sVBAT_SRAM_CODE = .;
  __sVBAT_SRAM_CODE__ = _sVBAT_SRAM_CODE;
  *(.VBAT_SRAM_CODE) /* All nominated variables */
  	. = ALIGN(4);
  _eVBAT_SRAM_CODE = .;
  __eVBAT_SRAM_CODE__ = _eVBAT_SRAM_CODE;
  } >VBAT_SRAM_CODE


  .VBAT_SRAM (NOLOAD) :  {
  . = ALIGN(4);
  _sVBAT_SRAM = .;
  __sVBAT_SRAM__ = _sVBAT_SRAM;
  *(.VBAT_SRAM) /* All nominated variables */
  	. = ALIGN(4);
  _eVBAT_SRAM = .;
  __eVBAT_SRAM__ = _eVBAT_SRAM;
  } >VBAT_SRAM


  /* Remove information from the compiler libraries */
  /DISCARD/ :
  {
    libc.a ( * )
    libm.a ( * )
    libgcc.a ( * )
  }

  .ARM.attributes 0 : { *(.ARM.attributes) }



  FontFlashSection :
  {
    *(FontFlashSection FontFlashSection.*)
    *(.gnu.linkonce.r.*)
    . = ALIGN(0x4);
  } >ASSETS_FLASH

  TextFlashSection :
  {
    *(TextFlashSection TextFlashSection.*)
    *(.gnu.linkonce.r.*)
    . = ALIGN(0x4);
  } >ASSETS_FLASH

  ExtFlashSection :
  {
    *(ExtFlashSection ExtFlashSection.*)
    *(.gnu.linkonce.r.*)
    . = ALIGN(0x4);
  } >ASSETS_FLASH

  BmpCacheSection (NOLOAD) : { *(BmpCacheSection) } >SDRAM_FB
  TouchGFX_Framebuffer (NOLOAD) : { *(TouchGFX_Framebuffer) } >SDRAM_FB
  TouchGFX_Framebuffer1 (NOLOAD) : { *(TouchGFX_Framebuffer1) } >SDRAM_FB
  TouchGFX_Framebuffer2 (NOLOAD) : { *(TouchGFX_Framebuffer2) } >SDRAM_FB
  Video_RGB_Buffer (NOLOAD) : { *(Video_RGB_Buffer) } >SDRAM_FB

}

/* Start-up code */

  .syntax unified
  .cpu cortex-m7
  .fpu softvfp
  .thumb

.global  g_pfnVectors
.global  Default_Handler

/* start address for the initialization values of the .data section. 
defined in linker script */
.word  _sidata
/* start address for the .data section. defined in linker script */  
.word  _sdata
/* end address for the .data section. defined in linker script */
.word  _edata
/* start address for the .bss section. defined in linker script */
.word  _sbss
/* end address for the .bss section. defined in linker script */
.word  _ebss
/* stack used for SystemInit_ExtMemCtl; always internal RAM used */

/**
 * @brief  This is the code that gets called when the processor first
 *          starts execution following a reset event. Only the absolutely
 *          necessary set is performed, after which the application
 *          supplied main() routine is called. 
 *   None
 * @retval : None
*/

    .section  .text.Reset_Handler
  .weak  Reset_Handler
  .type  Reset_Handler, %function
Reset_Handler:  
  ldr   sp, =_estack      /* set stack pointer */

/* Copy the data segment initializers from flash to SRAM */  
  movs  r1, #0
  b  LoopCopyDataInit

CopyDataInit:
  ldr  r3, =_sidata
  ldr  r3, [r3, r1]
  str  r3, [r0, r1]
  adds  r1, r1, #4
    
LoopCopyDataInit:
  ldr  r0, =_sdata
  ldr  r3, =_edata
  adds  r2, r0, r1
  cmp  r2, r3
  bcc  CopyDataInit
  ldr  r2, =_sbss
  b  LoopFillZerobss
/* Zero fill the bss segment. */  
FillZerobss:
  movs  r3, #0
  str  r3, [r2], #4
    
LoopFillZerobss:
  ldr  r3, = _ebss
  cmp  r2, r3
  bcc  FillZerobss

 

 

 

 

 

10 REPLIES 10

I was using cubeIDE v1.16.1. and I got the same issue in the live expression where my variables are shown with a memory offset of +8bits (i.e. corrupted values).

A month ago I got the same issue with a memory offset of +32bits in the live watch only.

Sometimes the issue is persistent, sometimes it disappears. I did not find the root cause until now.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.