2024-08-29 10:15 AM
Hello,
we bought a STM32H757 i-EVAL and I started to play with it. So I chose the board in STMCUBE MX (version 6.12.0) and selected the default configuration. After compiling code which went well, it got stuck in the MX_SDMMC1_SD_Init function, with the following error: HAL_SD_ERROR_UNSUPPORTED_FEATURE,
So after reviewing couple of posts here, i figured out that there is a mistake in auto-generated codes from Cube, so I changed "hsd1.Init.TranceiverPresent " to SDMMC_TRANSCEIVER_PRESENT instead of SDMMC_TRANSCEIVER_NOT_PRESENT. Here Sd init function now:
hsd1.Instance = SDMMC1;
hsd1.Init.ClockEdge = SDMMC_CLOCK_EDGE_RISING;
hsd1.Init.ClockPowerSave = SDMMC_CLOCK_POWER_SAVE_DISABLE;
hsd1.Init.BusWide = SDMMC_BUS_WIDE_4B;
hsd1.Init.HardwareFlowControl = SDMMC_HARDWARE_FLOW_CONTROL_DISABLE;
hsd1.Init.ClockDiv = 0;
hsd1.Init.TranceiverPresent = SDMMC_TRANSCEIVER_PRESENT;
To be honest, it seemed solved the problem but after couple of tests, it again crashes with the same error.
Any help would be highly appreciated. ( I have attached my .ioc file for reference)
Amir
Solved! Go to Solution.
2024-08-30 5:32 AM
Hello,
Try first to run the native example working on STM32H747I-EVAL board provided in the STM32CubeH7 in here: https://github.com/STMicroelectronics/STM32CubeH7/tree/master/Projects/STM32H747I-EVAL/Applications/FatFs/FatFs_Dual_Instance
At least to validate your SDcard.
2024-08-30 5:32 AM
Hello,
Try first to run the native example working on STM32H747I-EVAL board provided in the STM32CubeH7 in here: https://github.com/STMicroelectronics/STM32CubeH7/tree/master/Projects/STM32H747I-EVAL/Applications/FatFs/FatFs_Dual_Instance
At least to validate your SDcard.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.