2021-05-29 9:48 PM
I had a problem with the IDE and deleted it by manually searching all the files on my ubuntu 20.04.
Now when I try to run the binary again, it says "Nothing to install.", however I have deleted all stm files from my machine.
What can I do?
Solved! Go to Solution.
2021-05-30 11:43 PM
Hi,
Looks like STM32CubeIDE is still part of the native package manager database.
To check this assumption you can use the dpkg command:
dpkg -l '*stm32cubeide*'And then remove correctly the package using :
sudo dpkg -r st-stm32cubeide-1.x.xReplace the version token 1.x.x by the one reported in first dpkg query.
HTH
2021-05-30 11:43 PM
Hi,
Looks like STM32CubeIDE is still part of the native package manager database.
To check this assumption you can use the dpkg command:
dpkg -l '*stm32cubeide*'And then remove correctly the package using :
sudo dpkg -r st-stm32cubeide-1.x.xReplace the version token 1.x.x by the one reported in first dpkg query.
HTH
2021-06-11 11:11 PM
Isn't there a uninstaller under installation folder opt/ ?
2024-09-29 8:56 AM
To ST employee,
I was struggling with this issue for a while. I had to open the (heavy) script to understand why it does not install. Please make sure to at least issue a warning when the script detects that the package was already installed/available in system and ask user to uninstall (via dpkg). A basic warning should do, and this is fundamental.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.