2025-04-03 9:13 PM
Hi,
I am trying to build on STM32Cube IDE, it is showing that "make -j8 all" terminated with exit code -1. Build might be incomplete. Then while trying to flash or debug it is not working.
I tried to disable parallel build, but still this issue I am facing. But still the same issue.
I have attached the screenshot of the build output console for an example code.
Currently I am using this for STM32F429ZI-DISC1 board.
Could you please support here, if I am missing something for which this build issue is appearing.
Thank you for your support.
2025-04-03 11:04 PM
Can you enable full console output, or the run make from a command line ?
I suppose you will find more detailed error messages there.
And probably without the "-j8" option, or add '--output-sync' to have the outputs synchronized.
2025-04-07 7:08 PM
From the command line I tried running, but shows as "'make' is not recognized as an internal or external command,
operable program or batch file".
Tried without the "-j8" option, and adding '--output-sync' ,
but getting the same output as ""make --output-sync all" terminated with exit code -1. Build might be incomplete."
2025-04-08 11:13 PM
My point was to get ALL the console outputs, not just the summary.
And second, synchonized output is easier to read, but not essential in this case.
To do that, you might need to dig deeper into the documentation of your toolcain / IDE.
One of the reasons I personally do not use Cube.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.