2024-01-04 12:03 PM
Hello guys
My microcontroller is: STM32L432KCU6 - nucleo board
I have a problem with PWM. I need to change TIM16 to TIM15 because TIM16 collides with I2C
So thats why I have to use TIM15... I need him to handle micro servo. When i use TIM16, everything works, the pulses and the duty cycle are correct, but when i use TIM15, unfortunately the duty cycle is still 0
TIMx configurations:
Clock configuration:
There is a code that i use to handle micro servo, for TIM16 it works
int main(void) { /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_DMA_Init(); MX_TIM16_Init(); MX_TIM15_Init(); /* USER CODE BEGIN 2 */ HAL_TIM_PWM_Start(&htim16, TIM_CHANNEL_1); HAL_TIM_PWM_Start(&htim15, TIM_CHANNEL_2); /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { // TIM 16 ####################### htim16.Instance->CCR1 = 25; // 0 stopni HAL_Delay(2000); htim16.Instance->CCR1 = 50; // 45 stopni HAL_Delay(2000); htim16.Instance->CCR1 = 75; // 90 stopni HAL_Delay(2000); htim16.Instance->CCR1 = 110; // 153 stopnie HAL_Delay(2000); htim16.Instance->CCR1 = 125; // 180 stopni HAL_Delay(5000); // TIM 15 ####################### htim15.Instance->CCR2 = 25; // 0 stopni HAL_Delay(2000); htim15.Instance->CCR2 = 50; // 45 stopni HAL_Delay(2000); htim15.Instance->CCR2 = 75; // 90 stopni HAL_Delay(2000); htim15.Instance->CCR2 = 110; // 153 stopnie HAL_Delay(2000); htim15.Instance->CCR2 = 125; // 180 stopni HAL_Delay(5000); /* USER CODE END WHILE */ /* USER CODE BEGIN 3 */ } /* USER CODE END 3 */ } |
Is anyone know what going on?
2024-01-04 12:13 PM - edited 2024-01-04 12:17 PM
Your code doesn't output a TIM15 PWM signal until 13 seconds in. Are you waiting that long? Consider modifying TIM15 and TIM16 duty cycle at the same time.
Debug code, verify that TIM15->CNT is changing and that TIM15->CCR2 is updating appropriately.
2024-01-04 12:25 PM
At 80 MHz to get the TIM at 50 KHz you'd need a prescaler of 1600-1 not 1597
Although having a broader ARR of 20000-1 would give a lot finer resolution
Not showing initialization code, or pin configuration
Any conflicts on the pins used? Solder Bridge options, actually get to pin headers?
2024-01-04 12:39 PM
CNT is changing
I discovered that when I power the device via external power then duty cycle = 0%, and when I disconnect it and leave the micro usb I have duty cycle = correct
I have no idea where I might have a short circuit or something
2024-01-04 1:15 PM
Seems like an issue in how the servo is connected then, or other hardware issue with it. PC3 is free on that board.
2024-01-04 11:24 PM - edited 2024-01-04 11:28 PM
Read out and check/post relevant GPIO registers settings.
> PC3 is free on that board.
Why would we be talking about PC3?
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.