2023-10-13 6:48 AM
I have recently bought:
- a NUCLEO-F411RE board
- a X-NUCLEO-GFX01M2 TFT board
I work on Mac.
Unfortunatly, TouchGFXDesigner doesn't exist for Mac.
So I have installed STM32CubeIDE, STM32CubeProgrammer, and STM32CubeMX on my Mac.
I have installed TouchGFXDesigner on a Windows PC I can access to.
I have built a project on TouchGFXDesigner. It works fine with the simulator.
I want now to have this small project on my two boards.
So I have transfered the project directory from the PC to the Mac.
I have then launched STM32CubeProgrammer, and created a project from the directory received from the PC.
How can I now finish the project on the Mac, and transfer it to my boards.
In a first time, I just want to see what have been done on TouchGFXDesigner.
In fact, I don't see how associate the two boards, build the mini project, and upload it to the borads.
I'm completely new to STM32.
I have watched many videos on Youtube, read many docs, but I'm stuck doing this.
If someone could explain how to do, or point to a useful doc...
There are many examples but they all use other boards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.