2023-07-29 6:00 AM
I have custom PCB designed using STM32L476RG. I included SED 2x5 female connector so that I can program the board directly. How do I program it using STLINK - V3MINIE. Can I connect the debugger directly to the board without using any connection wires? Also It would be of great help if someone can explain me the process or the steps involved.
Thanks
Nikhila
2023-07-29 7:55 AM
If you have the appropriate header on your board, yes you:
Not sure what "SED 2x5 female connector" is, but it doesn't sound like the appropriate header, so you will need to find a way to connect GND, SWDIO, SWCLK between the two, at a minimum.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.