2024-12-09 8:53 AM - edited 2024-12-09 8:58 AM
Hi,
I got an issue where I can no longer activate SWV Viewer option inside debug configuration for my NUCLEO-U083RC board. The SWV checkbox is greyed out.
Whether I create a new project or load an existing one, the SWV option is greyed out and can no longer be selected.
Anyone got an idea what is going on?
Also I had some issues with ITM_SendChar as it would not compile.
Debug Trace Asynchronous Sw is active. On Nucleo board I assume SWO is connected.
Cube IDE 1.17.0.
STM32U0 V1.2 package.
Solved! Go to Solution.
2024-12-09 9:11 AM
Hello @chris84 ,
SWV is not available for the Cortex-M0, that is why the button to enable SWV option is greyed out.
Try to use Live Expressions if you want to check a specific variable for example.
2024-12-09 9:11 AM
Hello @chris84 ,
SWV is not available for the Cortex-M0, that is why the button to enable SWV option is greyed out.
Try to use Live Expressions if you want to check a specific variable for example.
2024-12-09 9:24 AM
Hi @Imen.D
thank you very much for quickly shed light on it.
The fact that in Cube MX under Debug I still can activate SWO as Trace Asynchronous Sw was misleading for me.
Thanks you. Chris
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.