2019-11-28 1:37 AM
Hi,
i am using STM32CubeIDe in my project. i am using STM32F030 as transmitter and STM32F4 as a receiver. When i run my code in debug mode both of them work properly. But when i press terminate and re-insert my ST-LINK device i can't see any data in my receiver (also i see that receiver and transmitter connects). How can i download the code and use it without debug mode?
Here is my code. (In main, there are only pin configurations, so i didn't post it)
#include "main.h" //buraya don
#include "stm32f0xx_hal.h"
#include "dht22.h"
uint8_t nem_byte1, nem_byte2, sicaklik_byte1, sicaklik_byte2,checksum, verilerin_toplami;
uint16_t nem, sicaklik,sicaklik1,nem1,timer_sayac_degeri;
void delay_ticks(uint32_t ticks)
{ //SYSTICK TIMER 24 BIT
SysTick->LOAD = ticks; //girilen süre için gerekli tick sayısı
SysTick->VAL = 0;
SysTick->CTRL = SysTick_CTRL_ENABLE_Msk;
SysTick->CTRL &= ~SYSTICK_CLKSOURCE_HCLK_DIV8;
SysTick->CTRL |= SYSTICK_CLKSOURCE_HCLK;
//COUNTFLAG,counter 0 oldugunda 1 oluyo.
//okundugunda otomatik oalrak temizleniyo
while ((SysTick->CTRL & SysTick_CTRL_COUNTFLAG_Msk) == 0);
SysTick->CTRL = 0;
}
void delay_us(uint32_t us)
{
delay_ticks(us * 8);
}
static inline void delay_ms(uint32_t ms)
{
delay_ticks(ms * 8000);
}
GPIO_InitTypeDef GPIO_InitStruct = {0};
void pini_giris_yap (void)
{
GPIO_InitStruct.Pin = GPIO_PIN_5;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
}
/*Configure GPIO pin : PA2 */
void pini_cikis_yap (void)
{
GPIO_InitStruct.Pin = GPIO_PIN_5;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
}
void DHT22_baslat (void)
{
pini_cikis_yap();
HAL_GPIO_WritePin (GPIOA, GPIO_PIN_5, 0); // baslangica sinyali
delay_us(1100);
HAL_GPIO_WritePin (GPIOA, GPIO_PIN_5, 1); // sensorden gelecek cevabi bekle
delay_us(30);
pini_giris_yap();
}
void sensorden_yanit_al (void)
{
delay_us(120); //datasheete gore 80-160 arasi bir deger
while ((HAL_GPIO_ReadPin (GPIOA, GPIO_PIN_5)));
}
uint8_t veri_oku(void)
{
uint8_t i,j;
for (j=0;j<8;j++)
{
while (!(HAL_GPIO_ReadPin (GPIOA, GPIO_PIN_5))); // pin 1 olana keder bekle
delay_us(40); // 50 yapinca calismiyo
if ((HAL_GPIO_ReadPin (GPIOA, GPIO_PIN_5)) == 0)
{
i&= ~(1<<(7-j)); // alinan bit 0
}
else i|= (1<<(7-j)); // alinan bit 1
while (HAL_GPIO_ReadPin (GPIOA, GPIO_PIN_5 && ((TIM3->CNT-timer_sayac_degeri)==1600) )); //problem olursa 200 us sonra devam et
}
return i;
}
void oku(void){
DHT22_baslat ();
sensorden_yanit_al ();
nem_byte1 = veri_oku();
nem_byte2 = veri_oku();
sicaklik_byte1 = veri_oku();
sicaklik_byte2 = veri_oku();
checksum = veri_oku();// check-sum should be the last 8 bit of "8 bit integral RH data+8 bit decimal RH
//data+8 bit integral T data+8 bit decimal T data".
verilerin_toplami=(nem_byte1+nem_byte2+sicaklik_byte1+sicaklik_byte2);
// HAL_UART_Transmit(&huart1,(uint8_t*)"resul\r\n",sizeof("resul\r\n")-1,100);
if ((checksum) == verilerin_toplami)
{
sicaklik = ((sicaklik_byte1<<8)|sicaklik_byte2);
nem = ((nem_byte1<<8)|nem_byte2);
}
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.