2019-11-04 11:45 PM
When generating code, files STM32H745ZITX_FLASH.ld are updated for CM4 and CM7
For CM4, I found :
/* Specify the memory areas */
MEMORY
{
FLASH (rx) : ORIGIN = 0x08100000, LENGTH = 1024K
RAM (xrw) : ORIGIN = 0x10000000, LENGTH = 288K
}
and for CM7 :
/* Specify the memory areas */
MEMORY
{
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 1024K
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
}
Available RAM is 1M for such a device, so the whole space is not used.
I can modify the script files, but it isn't a good issue because these files are re-generated automatically when my project is evolving.
Could the IDE allow to define memory spaces ? (and well defined by default)
2020-05-25 10:18 PM
Is there anything new for this issue?
2020-05-25 10:42 PM
Generally one needs to address these things directly as they involve complex interactions.
Modify the linker scripts to suit your memory floorplan.
Add code in startup.s to enable the memory clocks and unpack the load regions and statics you've described in the linker script.
If you use the heap you'll need to check that the _sbrk allocator understands the memory map and the heap / stack relationship properly.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.