cancel
Showing results for 
Search instead for 
Did you mean: 

Keyboard keys stop working at random STM32CubeIDE Linux

Dabbo
Associate III

I use STM32CubeIDE on Linux Ubuntu (and to a lesser extent on MacOS and Windows, but I don't recall having a problem on the last 2 operating systems). About once or twice a day, at random, several of the keys such as <backspace> and <enter> and <delete> stop working. All the alphabetical and number keys work as normal. If I switch to a different application all the keys are working, but when I switch back to Cube the problem continues.

I solve the problem by saving my work, shutting and relaunching Cube. Is this a bug in the application?

15 REPLIES 15

Hi!

Are there any updates to this issue? As of 1 September 2024, this issue is still present on the Ubuntu operating system.

Hello,

I suggest that you download the last version of STM32CubeIDE through this link:

STM32CubeIDE - Integrated Development Environment for STM32 - STMicroelectronics.

In fact, this issue does not exist anymore on STM32CubeIDE 1.16.0 ; Ubuntu 22.04.

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

It still exists with 1.16.1; Ubuntu 22.04

Zipper
Associate II

I'm still experiencing a similar problem on the latest version (6.17.0) on Debian sid with Cinnamon. Though in my case the keyboard stops working entirely. I can't enter any text and keybinds like CTRL+S don't work either. It's coupled with very slow startup times of the program. Strangely it only manifests on my laptop and not on my desktop PC with the same OS and desktop environment.


@Zipper wrote:

I'm still experiencing a similar problem on the latest version (6.17.0) .


That sounds like a CubeMX version ?

Is only your CubeMX affected, or also CubeIDE - if so, what version?

 


@Zipper wrote:

 in my case the keyboard stops working entirely. .


as in, for all apps - not just Cube-related ?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

I came from a search and someone failed to see this is about CubeIDE. How silly. This problem indeed only affects CubeMX, not CubeIDE.