2024-05-15 9:40 AM
Hello,I tried to use a J-Trace to program an STM32U5G9J-DK1. This J-Trace Pro works well on other projects. I also tried a J-link and it shows the same issue. While, of course, STLink3 via the same connector works well.After I look into the J-link log file, the J-link driver in the latest 1.5.1 IDE is still V7.94h. Even my PC has the latest j-link v7.96g, the IDE will not automatically upgrade. The J-link release notes shows the STM32U5G9 was supported since v7.94m. I feel that could be the reason why the IDE doesn't recognize the DK.I overwrote the bin folder (C:\ST\STM32CubeIDE_1.15.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.jlink.win32_2.2.200.202402092224\tools) by the the entire v7.96g J-link folder. The the IDE showed the v7.96g was loaded, but it pops a different error.Is there a correct way I can manually upgrade the J-link driver embedded in the IDE?Both j-link logs are posted below,Thank you very much!The first J-link Log based on v7.94h:----------------------------------------------------------------------------SEGGER J-Link GDB Server V7.94h Command Line Version
JLinkARM.dll V7.94h (DLL compiled Feb 1 2024 11:04:36)
Command line: -port 2331 -s -device STM32U5G9NJ -endian little -speed 4000 -if swd -vd
-----GDB Server start settings-----
GDBInit file: none
GDB Server Listening port: 2331
SWO raw output listening port: 2332
Terminal I/O port: 2333
Accept remote connection: localhost only
Generate logfile: off
Verify download: on
Init regs on start: off
Silent mode: off
Single run mode: on
Target connection timeout: 0 ms
------J-Link related settings------
J-Link Host interface: USB
J-Link script: none
J-Link settings file: none
------Target related settings------
Target device: STM32U5G9NJ
Target device parameters: none
Target interface: SWD
Target interface speed: 4000kHz
Target endian: little
Connecting to J-Link...
J-Link is connected.
Failed to get index for device name 'STM32U5G9NJ'.GDBServer will be closed...
Shutting down...
Could not connect to target.
Please check power, connection and settings.
-----------------------------------------------------------The second J-link Log by v7.96----------------------------------------------------------SEGGER J-Link GDB Server V7.96g Command Line Version
JLinkARM.dll V7.96g (DLL compiled May 8 2024 15:00:44)
Command line: -port 2331 -s -device STM32U5G9NJ -endian little -speed 4000 -if swd -vd
-----GDB Server start settings-----
GDBInit file: none
GDB Server Listening port: 2331
SWO raw output listening port: 2332
Terminal I/O port: 2333
Accept remote connection: localhost only
Generate logfile: off
Verify download: on
Init regs on start: off
Silent mode: off
Single run mode: on
Target connection timeout: 0 ms
------J-Link related settings------
J-Link Host interface: USB
J-Link script: none
J-Link settings file: none
------Target related settings------
Target device: STM32U5G9NJ
Target device parameters: none
Target interface: SWD
Target interface speed: 4000kHz
Target endian: little
Connecting to J-Link...
J-Link is connected.
Firmware: J-Trace PRO V3 Cortex-M compiled Apr 25 2024 09:13:57
Hardware: V3.00
S/N: 753002352
Feature(s): RDI, FlashBP, FlashDL, JFlash, GDB
Checking target voltage...
Target voltage: 1.75 V
Listening on TCP/IP port 2331
Connecting to target...
ERROR: Could not connect to target.
Target connection failed. GDBServer will be closed...Restoring target state and closing J-Link connection...
Shutting down...
Could not connect to target.
Please check power, connection and settings.
------------------------------------
Solved! Go to Solution.
2024-05-15 12:37 PM
Well, after rebooting everything, suddenly the IDE + J-trace can program the DK.
Yes, still need update the J-link to the latest version, but the way to update was correct.
Request closed!
2024-05-15 12:37 PM
Well, after rebooting everything, suddenly the IDE + J-trace can program the DK.
Yes, still need update the J-link to the latest version, but the way to update was correct.
Request closed!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.