2020-06-24 1:27 AM
I found a selection option under Properties->C/C++ Build->Settings-> Toolchain Version
but this only allows to select two STM32CubeIDE internal gnu arm gcc toolchains.
It'd be nice if one could select an external path with a newer GNU Arm Embedded Toolchain.
2020-06-24 6:13 AM
You might want to post it in the Idea Zone. I will upvote it there.
2020-06-24 6:31 AM
You can change the path variable used for the compiler such that it sees the newer toolchain first, and it'll use that. Not ideal, but it does work.
2020-08-03 4:44 PM
This would be very good. We use an automated build server and so would like to locally build using a specific toolchain version. Currently we have to manually edit the PATH in each project we build, and this changes for every person that works on those projects, so a bit of a version control nightmare. I've created a post in the Idea Zone (didn't see one from OP).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.