2023-11-30 6:31 AM
Board H745ZI
I have installed ARM.CMSIS 5.8.0 and CMSIS-DSP 1.15.0 via the IOC>Software packs> and selected the components I want available under Select components. I have then enabled them under Middleware and software packs so CMSIS and CMSIS-DSP are both green and ticked. I have clicked the generate code icon and I can see ARM_CMSIS under Middlewares>Third_Party>ARM_CMSIS and under Middlewares>Third_Party>ARM_CMSIS>Source I can see a bunch of the source files for DSP functions. The weird thing is that a whole bunch of functions are missing. So if I clean the project (just to check the compiler can see all of the required files) I get a bunch of errors.
What I do not understand is STM32CUBEIDE is clearly looking in the correct place, it just seems not all the files have been copied over from the pack repository.
Can someone help?
2023-11-30 6:38 AM
Hello @MEde.1,
I recommend you following this article: Configuring DSP libraries on SM32CubeIDE, it would help you.
Imen
2023-11-30 6:39 AM
I'll take a look. If I use the dev DSP under CMSIS (as opposed to CMSIS-DSP) everything is fine.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.