2023-07-25 1:24 PM
I am using STM32CubeIDE to develop applications on the STM32H563 processor, and I need to use the LWIP (Lightweight IP) library to manage network communication.
However, I cannot find the LWIP library in the list of Middlewares available in STM32CubeIDE.
I would like to know if the LWIP library is supported for the STM32H563 processor in STM32CubeIDE, and if so, how can I include it in my project?
Thank you in advance for your assistance and clarification on this matter.
Best regards.
2023-07-25 2:38 PM
It is _not_ supported by ST (currently) and yes, you are free to download it from its home site or other STM32 package, and use.
If this seems confusing or too much hassle, outsource it.
2023-07-26 3:59 PM
Why are you creating a duplicate topics?
Effectively it doesn't matter whether they "support" it, because their code is a broken bloatware anyway:
2023-07-27 4:17 AM
Dear Piranha,
Did you hear anything from them (STM32 team) yet for following topic ?
I believe they had committed to fix it by June-2023. I took multiple follow up in the same thread. No response from them yet.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.