2024-06-07 11:28 AM - last edited on 2024-06-07 2:12 PM by Tesla DeLorean
Hi Community,
I am working on a project with a custom board that uses both HSE (24MHz) and LSE (32.768KHz) clock sources. TIM6 is used as a time base source because SysTick is used by the RTOS. When running a debug session I can see that it is going into an infinite loop at the following code in the HAL library.
/* Wait till LSE is ready */
while (READ_BIT(RCC->BDCR, RCC_BDCR_LSERDY) == 0U)
{
if((HAL_GetTick() - tickstart) > RCC_LSE_TIMEOUT_VALUE)
{
return HAL_TIMEOUT;
}
}
After a closer look, it is found that HAL_GetTick is returning 0 every time because of which it went into an infinite loop but it should not be zero at this point because it is initialized in the HAL_Init with HAL_InitTick which in turn runs TIM6 ISR and should start updating the tick.
Why is that so?
PS: The configuration and code generation is done using STM32CubeIDE. This code ran effectively on a Nucleo Board. But not running on a custom board.
2024-06-16 11:05 PM
Hi,
set the LSE drive to high drive , check then in program.
Be aware if check with a scope: with 10:1 (10Mohm) probe it might be possible, to see the 32kHz oscillation, but you might stop it, just because connecting the probe !
And the crystal + surrounding area has to be clean, no solder/flux remains there; clean with aceton or isopropanol, if not sure about "clean" .
+ check Vbat : > 3.0 V ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.