2020-01-26 10:49 PM
Hi,
I am using STM32CubeIDE for audio application development. In my application STM32 will be working as I2S Master Receiver so I wanted to collect data continuously without losing any data.
I have configured DMA with circular mode enabled.
Looking at some document with respect to stm32, I have got an answer that when we configure circular mode then DBM bit from DMA_SxCR Register should be set and followed by second memory address. but auto code genrated by the tool does not allowing for circular transfer.
DMA_SxCR -> DBM bit is set with 0 in the DMA_SetConfig function.
Can anyone help me this ASAP.
I have to avoid data loss because it is an Audio application.
Regards,
Suresh.
2020-01-27 1:22 AM
If you don't plan to change the buffers' location, you don't need to use the double-buffer mode, you can achieve a similar result simply by using both the half-complete and transfer-complete interrupts.
JW
2020-01-27 1:55 AM
Hi Jan,
Thanks for your suggestion.
With your suggestion I have to select use_fifo mode with half full right?
In case If i want to use two different buffer how can i do that?
Regards,
Suresh.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.