2025-03-25 3:16 AM - edited 2025-03-25 3:18 AM
I have a problem when typing code on stm32cube ide on macos. For example, when I type the word int, there will be a blue underline under int. If I press enter or space, the blue underline will disappear. I press enter again and it will go to the next line and the word int will not be deleted. And if the blue underline is lost, I can move the mouse to another line normally without losing the word int. If there is still a blue line, when I move the mouse to another line, the word int will be deleted. The same goes for deletion. When I finish writing the word int and press delete immediately, the first letter in the word int, the letter i, will be deleted. All the commands or documents I write in here have these 2 errors. If anyone has this problem, please help me.
Thank you!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.