2024-09-29 12:12 PM
When I try to install it I get this error: "The following packages have unmet dependencies:
st-stm32cubeide-1.16.1 : Depends: libncurses5 but is not installable
Depends: libpython2.7 but is not installable
Depends: libwebkit2gtk-4.0-37 but is not installable"
any ideas? thanks in advance
Solved! Go to Solution.
2024-10-04 1:42 AM
Hi,
Try the generic version of 1.16.0, then update through CubeIDE's updater. That worked for me on Tumbleweed.
I hope that helps.
Kind regards
Pedro
2024-10-04 1:47 AM - edited 2024-10-04 1:48 AM
Hi,
Good news that can work, maybe something slightly different create the issue for me and a lot of people...
Which distribution of Linux are you using ?
Indeed, I already tried 1.16.0 before, 'arm-none-eabi-gdb' also requires libncurses5 (thus very specific version of it which doesn't really make sense for me). I tried 1.16.1 hopping it would had been fixed.
I see two solutions, get a newer generic 'arm-none-eabi-gdb' and replaced it in STMCubeIDE.
Use Archlinux... which integrate a packet creating a compatibility layer between libncurses5 and libncurses6, but I tend to avoid using Archlinux on my work computer.
Initially I had to migrate from the previous Ubuntu LTS to newer for very complex issues with Virtual Box...
Best regards.
2024-10-04 1:49 AM
PS: my system has NCURSES 5 installed...
2024-10-04 1:53 AM
Thanks PGump.1, that's indeed a very logical way for it to work... it's the third option.
I really want to avoid adding manually a deprecated lib (libncurses 6 exists since more or less 2018, and 6.1 date back 2020 so it's quite logical to deprecated libncurses 5).
2024-10-04 9:42 PM
@ValereAq I have had my system for a few years. I can't remember ever installing NCURSES 5. My system must have evolved that way...
Good luck.
Kind regards
Pedro
2024-10-10 3:50 AM
Because Ubuntu 24.04 doesn't have those library versions. The best thing would be for ST to rebuild the tools for the 24.04 version of Ubuntu. I got the same error on my new Ubuntu 24.04 installation. Luckily, I have another machine with the previous LTS version of Ubuntu (22.04 Jammy Jellyfish). The STM32VCubeIDE install worked fine there. I used the Linux zip and not the deb file. I don't have any reason to believe that the deb version would not work on 22.04 ... I just have not tried it.
2024-10-19 7:15 AM
A quick temporary solution, tested on arm-none-eabi-gdb:
# create local path to store softlink to ncurses6, avoid sudo, also doesn't introduce
# files into a system directory
mkdir -p ~/path/to/some/dir
cd ~/path/to/some/dir
# whole idea is to make soft links libncursesw.so.5 -> /usr/lib/x86_64-linux-gnu/libncursesw.so.6
# check the version installed in your system-wide ncurses library
ln -s /usr/lib/x86_64-linux-gnu/libtinfo.so.6 libtinfo.so.5
ln -s /usr/lib/x86_64-linux-gnu/libncursesw.so.6 libncursesw.so.5
# try to execute, should work
LD_LIBRARY_PATH=~/path/to/some/dir arm-none-eabi-gdb
# to make systemwide, add LD_LIBRARY_PATH to your startup script, eg ~/.profile
# do not forget to substitute '~' with $HOME
export LD_LIBRARY_PATH=$HOME/path/to/some/
I didn't found a proper code highlight for SH script so used a python, should be readable...
2024-10-20 9:29 AM
ciao
I tried your code but it doesn't find the directory it gives me the following error
:~/path/to/some/dir$ LD_LIBRARY_PATH=~/path/to/some/dir arm-none-eabi-gdb
arm-none-eabi-gdb: comando non trovato
2024-10-29 10:43 PM
1.16.1 works fine on 24.10 for me. There is a conflict between FreeCAD 0.21, Kicad 8etc.. for Libncurses though. Perhaps uninstall those from the repository, then install CubEIDE again. On 24.04/10 you need to apply the ulimit though (see sticky post). I run FreeCAD, Kicad 8 an CubeIDE w/o problems on 24.10 now.
2025-04-15 9:47 PM - edited 2025-04-15 10:38 PM
On a fresh new installation of Ubuntu 24.04 I was able to install STM32CubeIDE v.1.18.0 and STM32CubeProgrammer v2.19.0 with no issues.
When asked to install Packages needed for some "Developer Package" use cases, instead of NCURSES 5 install NCURSES 6:
sudo apt-get install build-essential libncurses-dev libncurses6 libyaml-dev libssl-dev We’re moving the ST Community to a new platform to give you a better and more reliable community experience.