2020-02-19 11:06 PM
This is what CubeMX has generated for STM32F103VE mcu for LL GPIO driver:
#define LL_GPIO_PIN_0 ((GPIO_BSRR_BS0 << GPIO_PIN_MASK_POS) | 0x00000001U) /*!< Select pin 0 */
#define LL_GPIO_PIN_1 ((GPIO_BSRR_BS1 << GPIO_PIN_MASK_POS) | 0x00000002U) /*!< Select pin 1 */
#define LL_GPIO_PIN_2 ((GPIO_BSRR_BS2 << GPIO_PIN_MASK_POS) | 0x00000004U) /*!< Select pin 2 */
#define LL_GPIO_PIN_3 ((GPIO_BSRR_BS3 << GPIO_PIN_MASK_POS) | 0x00000008U) /*!< Select pin 3 */
#define LL_GPIO_PIN_4 ((GPIO_BSRR_BS4 << GPIO_PIN_MASK_POS) | 0x00000010U) /*!< Select pin 4 */
#define LL_GPIO_PIN_5 ((GPIO_BSRR_BS5 << GPIO_PIN_MASK_POS) | 0x00000020U) /*!< Select pin 5 */
#define LL_GPIO_PIN_6 ((GPIO_BSRR_BS6 << GPIO_PIN_MASK_POS) | 0x00000040U) /*!< Select pin 6 */
#define LL_GPIO_PIN_7 ((GPIO_BSRR_BS7 << GPIO_PIN_MASK_POS) | 0x00000080U) /*!< Select pin 7 */
#define LL_GPIO_PIN_8 ((GPIO_BSRR_BS8 << GPIO_PIN_MASK_POS) | 0x04000001U) /*!< Select pin 8 */
#define LL_GPIO_PIN_9 ((GPIO_BSRR_BS9 << GPIO_PIN_MASK_POS) | 0x04000002U) /*!< Select pin 9 */
#define LL_GPIO_PIN_10 ((GPIO_BSRR_BS10 << GPIO_PIN_MASK_POS) | 0x04000004U) /*!< Select pin 10 */
#define LL_GPIO_PIN_11 ((GPIO_BSRR_BS11 << GPIO_PIN_MASK_POS) | 0x04000008U) /*!< Select pin 11 */
#define LL_GPIO_PIN_12 ((GPIO_BSRR_BS12 << GPIO_PIN_MASK_POS) | 0x04000010U) /*!< Select pin 12 */
#define LL_GPIO_PIN_13 ((GPIO_BSRR_BS13 << GPIO_PIN_MASK_POS) | 0x04000020U) /*!< Select pin 13 */
#define LL_GPIO_PIN_14 ((GPIO_BSRR_BS14 << GPIO_PIN_MASK_POS) | 0x04000040U) /*!< Select pin 14 */
#define LL_GPIO_PIN_15 ((GPIO_BSRR_BS15 << GPIO_PIN_MASK_POS) | 0x04000080U) /*!< Select pin 15 */
#define LL_GPIO_PIN_ALL (LL_GPIO_PIN_0 | LL_GPIO_PIN_1 | LL_GPIO_PIN_2 | \
LL_GPIO_PIN_3 | LL_GPIO_PIN_4 | LL_GPIO_PIN_5 | \
LL_GPIO_PIN_6 | LL_GPIO_PIN_7 | LL_GPIO_PIN_8 | \
LL_GPIO_PIN_9 | LL_GPIO_PIN_10 | LL_GPIO_PIN_11 | \
LL_GPIO_PIN_12 | LL_GPIO_PIN_13 | LL_GPIO_PIN_14 | \
LL_GPIO_PIN_15) /*!< Select all pins */When I compile it in CubeIDE I get this warning:
large integer implicitly truncated to unsigned type [-Woverflow]
I am using latest version of libraries and CubeMX and CubeIDE.
I had also some problems using pins with number 8 and bigger to control GPIO.
Re-generation of code didn't solve the problem.
2022-11-03 11:05 AM
I have same problem, any solution?
2025-04-15 4:30 AM
Same problem in 2025. STMCubeMX Version 6.14.1.
2025-04-15 5:07 AM
Hello @edsontomioka ,
First let me thank you for posting and welcome to the ST Community.
For more investigation, I suggest please that you provide your Ioc.File.
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-04-15 2:25 PM
Sorry, the LLdriver is working fine. My fault.
I used _Pin for direct BSRR register access, but the LL driver _Pin definition is 32 bit unlike HAL driver 16 bit.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.