cancel
Showing results for 
Search instead for 
Did you mean: 

I am using STM32L081CB controller with 128K flash and want to change STM32L081CZ with 192K Flash. I don't find any direct option to change the same in the STMCUBE. I want the entire project remains same including the PIN mapping.

ADAS.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Uwe Bonnes
Chief

As long as you do not want to use memory or devices only in STM32L081CZ, use the binary produced for STM32L081CB for both.

MM..1
Chief III

And edit ld file to set larger flash

Uwe Bonnes
Chief

No need to change linker if there is no need for the additional flash...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.