2020-03-04 8:39 AM
2020-03-05 8:14 AM
OK, I found:
I need to set the GPIO's of my target uc in cube IDE (the cube MX part) to the debugger pins.
Then the
__HAL_AFIO_REMAP_SWJ_DISABLE();
is replaced by
__HAL_AFIO_REMAP_SWJ_ENABLE();
The deubgger still does not work in Cube IDE, but it works on the same environment flawlessly with Ozone.
So now I use Cube Ide for compiling and flashing, and Ozone for debugging.
That works for now.
2020-03-04 9:43 AM
Use STM32CubeProgrammer for that.
2020-03-05 7:42 AM
Thank you for the quick reply, highly appreciated.
Unfortunately there is a misunderstanding, due to my briefness in asking.
I dont't really want to set the option bytes. I want to AVOID them to be set.
Cube ide somehow does something strange here, which I want to understand and control:
When I use cube ide and start debugging, my device gets locked,
and is then not programmable/debuggable any more, unless I set BOOT0 low.
So, I need to find what is happening in cube ide.
(I am a beginner with cube ide - with the curent 1.3.0 version things start to be usable,
but in the past I had too much trouble, so I never really used it before).
2020-03-05 7:52 AM
My investigation so far shows that my problem is related to the
__HAL_AFIO_REMAP_SWJ_DISABLE();
call, which is generated by cube ide.
I found some other discussion in www about this.
I continue investigating ...
2020-03-05 7:56 AM
When BOOT0 is not low, the chip will boot from internal system memory (ROM) and listen on some interfaces for a boot loader. This feature is ment for firmware upgrade in the field, but not for debugging. Some chips have a option bit in flash for turing that BOOT0 pin behaviour off.
But AFAIK STM32CubeIDE does never mess with option bytes. Use STM32CubeProgrammer for option bytes inspection.
hth
KnarfB
2020-03-05 8:14 AM
OK, I found:
I need to set the GPIO's of my target uc in cube IDE (the cube MX part) to the debugger pins.
Then the
__HAL_AFIO_REMAP_SWJ_DISABLE();
is replaced by
__HAL_AFIO_REMAP_SWJ_ENABLE();
The deubgger still does not work in Cube IDE, but it works on the same environment flawlessly with Ozone.
So now I use Cube Ide for compiling and flashing, and Ozone for debugging.
That works for now.
2020-03-05 8:20 AM
Again thanks for the quick response and paying attention to this.
Sorry my mistake, I mean: "set Boot0 High".
I found what was going on by debugging and then stepping over the
__HAL_AFIO_REMAP_SWJ_DISABLE();
instruction, where the debugger said good bye.
And from here:
https://medium.com/@LargeCardinal/how-to-bypass-debug-disabling-and-crp-on-stm32f103-7116e7abb546
and here:
https://community.st.com/s/question/0D50X00009XkdjtSAB/bug-cubemx-switch-off-jtag-and-swd
I figured it out.
I posted my solution.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.