2023-09-09 5:09 PM
Newbie with STM32CubeIDE here, so apologies if this is a trivial question ;)
How do I use the sample Project code in the FP-SNS-DATALOG1 repo to build the hsdatalog application for the STWIN Starter Kit, STEVAL-STWINKT1B (SensorTile Wireless Industrial Mode)?
I probably don't need to rebuild this app -- pre-built binaries are provided and I can exercise the kit using them with json config files, but I definitely prefer to be able to examine and build the code I use. And I also want to use the STM32Cube IDE vs the alternatives.
So, what do I need to do to load and build the referenced project?
TIA,
Mike
2023-09-10 12:14 AM - edited 2023-09-10 12:15 AM
Hello @mikew67
I suggest you to install the last version of CubeMX and the last version of your firmware fp-sns-datalog1 (using the firmware installer of CubeMX) and then open the exemple from cube Mx in any IDE you want CubeIDE, keil, IAR).
Best regards.
II
2023-09-11 2:47 AM
Hello @mikew67 ,
After downloading FP-SNS-DATALOG1 repo, could you please import the project "en.fp-sns-datalog1\STM32CubeFunctionPack_DATALOG1_V1.5.0\Projects\STM32L4R9ZI-STWIN\Applications\HSDatalog\STM32CubeIDE" by following the steps in UM2609 - Rev 9 Section 2.10 Importing existing projects.
I hope this help you!
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.