2020-02-01 6:59 AM
1) How can I burn an STM project into the STMF767ZI in the STMCUBEIDE32 after I build the project?
2) The Debug isn't working:
STMicroelectronics ST-LINK GDB server. Version 5.2.3
Copyright (c) 2019, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
Target unknown error 19
Error in initializing ST-LINK device.
Reason: Unknown. Please check power and cabling to target.
Can somebody guide me how to install the ST-LINK?
I thought I did, I need help step by step please.
2020-02-01 10:53 AM
A custom board, or a Nucleo?
For the external ST-LINK make sure pin 1/2 have power for the buffers on the pod.
A non-functional chip/board will not be able to connect.
Check connections.
Check level on NRST.
Check power applied to VDDA.
Check voltages/capacitors on VCAP pins.
Do ST-LINK Utilities, or STM32 Cube Programmer find the chip?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.