cancel
Showing results for 
Search instead for 
Did you mean: 

How are you suposed to replicate a project???

sgordon777
Associate III
It's a pretty common need in an IDE to be able to branch or "fork" a project. Normall, I'd make a copy of the projet at the file level, then rename the original and continue development on that. However, Ranaming a project not only crashes, but also leaves the project broken: I don't see any "Save Project As" Option either.
I could make a copy and find every refeferenc to the project's name and change it, but this is tedious and error prone. Is there some way to do this I'm not seeing??
 
Error message I got when I Right-click project and "Rename"
sgordon777_0-1703350703203.png

 

Motor control workbench Version: 6.2.0
STM32CubeMX Version: 6.10.0
STM32CubeIDE Version: 1.14.0
Board: NUCLEO-G431-RB
 
 
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
AScha.3
Super User

Just try :  in IDE , left side, click on a project (selected = blue) , right click on it and select > copy< .

AScha3_0-1703352549263.png

then (on empty space i did) : right click and select > paste < .  -> give mod. name for new copy ->

AScha3_1-1703352694249.png

open here,  right click on xx.ioc and select > rename < .  -> give matching new mod. name for new copy 

AScha3_2-1703352837532.png

also rename xx debug + xx.launch

AScha3_1-1703354964514.png

+ in debug configurations ..main page for new debug->

AScha3_0-1703354894448.png

rename Name , Project, xx.elf

 

Then mod new xx.ioc , gen code, compile.... and TEST debug. :)

If you feel a post has answered your question, please click "Accept as Solution".
xisco
Senior

Hi,

I do it in the following way in CubeIDE:

1. File -> New ->STM32 project from an existing STM32CubeMX configuration file (ioc)

CubeIDE ask for ioc file and New Project name.

2. Copy includeFiles.c and main.c from OldProject/core/src to NewProject/core/src (overwriting main.c)

3. Copy includeFiles.h and main.h from OldProject/core/inc to NewProject/core/inc (overwriting main.h)

 

 

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.