2021-05-19 11:08 AM
these are the functions
__asm void my_strcpy(const char *src, char *dst)
{
loop
LDRB r2, [r0] ; Load byte into r2 from memory pointed to by r0 (src pointer)
ADDS r0, #1 ; Increment src pointer
STRB r2, [r1] ; Store byte in r2 into memory pointed to by (dst pointer)
ADDS r1, #1 ; Increment dst pointer
CMP r2, #0 ; Was the byte 0?
BNE loop ; If not, repeat the loop
BX lr ; Else return from subroutine
}
__asm void my_capitalize(char *str)
{
cap_loop
LDRB r1, [r0] ; Load byte into r1 from memory pointed to by r0 (str pointer)
CMP r1, #'a'-1 ; compare it with the character before 'a'
BLS cap_skip ; If byte is lower or same, then skip this byte
CMP r1, #'z' ; Compare it with the 'z' character
BHI cap_skip ; If it is higher, then skip this byte
SUBS r1,#32 ; Else subtract out difference to capitalize it
STRB r1, [r0] ; Store the capitalized byte back in memory
cap_skip
ADDS r0, r0, #1 ; Increment str pointer
CMP r1, #0 ; Was the byte 0?
BNE cap_loop ; If not, repeat the loop
BX lr ; Else return from subroutine
}
The GNU compiler doesnt accept these functions
Please can you tell how to change these functions?
Best regards and thanks in advance
Horacio Merovich
Solved! Go to Solution.
2021-05-19 5:51 PM
Honestly I despair the state of post-secondary education... is there not someone qualified to lead the course?
/* GNU/GAS Assembler code added into startup.s */
/* extern void my_strcpy(const char *src, char *dst); note parameters backward compared to C */
.section .text.my_strcpy
.type my_strcpy, %function
my_strcpy:
loop:
LDRB r2, [r0] /* Load byte into r2 from memory pointed to by r0 (src pointer) */
ADD r0, #1 /* Increment src pointer */
STRB r2, [r1] /* Store byte in r2 into memory pointed to by (dst pointer) */
ADD r1, #1 /* Increment dst pointer */
CMP r2, #0 /* Was the byte 0? */
BNE loop /* If not, repeat the loop */
BX lr /* Else return from subroutine */
.size my_strcpy, .-my_strcpy
/* extern void my_capitalize(char *str); */
.section .text.my_capitalize
.type my_capitalize, %function
my_capitalize:
cap_loop:
LDRB r1, [r0] /* Load byte into r1 from memory pointed to by r0 (str pointer) */
CMP r1, #'a'-1 /* compare it with the character before 'a' */
BLS cap_skip /* If byte is lower or same, then skip this byte */
CMP r1, #'z' /* Compare it with the 'z' character */
BHI cap_skip /* If it is higher, then skip this byte */
SUB r1,#32 /* Else subtract out difference to capitalize it */
STRB r1, [r0] /* Store the capitalized byte back in memory */
cap_skip:
ADD r0, r0, #1 /* Increment str pointer */
CMP r1, #0 /* Was the byte 0? */
BNE cap_loop /* If not, repeat the loop */
BX lr /* Else return from subroutine */
.size my_capitalize, .-my_capitalize
/* ... */
2021-05-19 1:25 PM
Start by replacing this with standard C library functions, strcpy (or better strncpy) and strupr.
Optimize later, when the project is working.
-- pa
2021-05-19 2:39 PM
Thanks for your answer
This code is part of a ARM Assembler course so we dont want to use here the standard C library functions.
Best regards
2021-05-19 5:51 PM
Honestly I despair the state of post-secondary education... is there not someone qualified to lead the course?
/* GNU/GAS Assembler code added into startup.s */
/* extern void my_strcpy(const char *src, char *dst); note parameters backward compared to C */
.section .text.my_strcpy
.type my_strcpy, %function
my_strcpy:
loop:
LDRB r2, [r0] /* Load byte into r2 from memory pointed to by r0 (src pointer) */
ADD r0, #1 /* Increment src pointer */
STRB r2, [r1] /* Store byte in r2 into memory pointed to by (dst pointer) */
ADD r1, #1 /* Increment dst pointer */
CMP r2, #0 /* Was the byte 0? */
BNE loop /* If not, repeat the loop */
BX lr /* Else return from subroutine */
.size my_strcpy, .-my_strcpy
/* extern void my_capitalize(char *str); */
.section .text.my_capitalize
.type my_capitalize, %function
my_capitalize:
cap_loop:
LDRB r1, [r0] /* Load byte into r1 from memory pointed to by r0 (str pointer) */
CMP r1, #'a'-1 /* compare it with the character before 'a' */
BLS cap_skip /* If byte is lower or same, then skip this byte */
CMP r1, #'z' /* Compare it with the 'z' character */
BHI cap_skip /* If it is higher, then skip this byte */
SUB r1,#32 /* Else subtract out difference to capitalize it */
STRB r1, [r0] /* Store the capitalized byte back in memory */
cap_skip:
ADD r0, r0, #1 /* Increment str pointer */
CMP r1, #0 /* Was the byte 0? */
BNE cap_loop /* If not, repeat the loop */
BX lr /* Else return from subroutine */
.size my_capitalize, .-my_capitalize
/* ... */
2021-05-20 6:10 AM
Hi
Thanks for your contribution to improve our education.
Best regards
Horacio
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.