2020-10-08 1:17 AM
I have developed a project in Keil Microvision v5.and the program is successfully compiled and running. But when I run the same program using Cube IDE v1.4.2 there are some warnings and when I flash the coding the system hangs .I have attached details regarding the warnings.
C:/Users/Dell/Documents/Mxcube/CPU_test_08_10_20/serial.c:35:26: warning: format '%X' expects argument of type 'unsigned int', but argument 3 has type 'uint32_t {aka long unsigned int}' [-Wformat=]
sprintf(buffer,"%08X", commend_data);
~~~^
%08lX
In file included from ../Core/Src/main.c:35:0:
C:/Users/Dell/Documents/Mxcube/CPU_test_08_10_20/subfunction.c: In function 'card_int':
C:/Users/Dell/Documents/Mxcube/CPU_test_08_10_20/subfunction.c:10:24: warning: assignment from incompatible pointer type [-Wincompatible-pointer-types]
sendcyp1=&Encryptedtext[0];
^
C:/Users/Dell/Documents/Mxcube/CPU_test_08_10_20/subfunction.c:11:22: warning: assignment from incompatible pointer type [-Wincompatible-pointer-types]
sendcyp2=&Encryptedtext[1];
^
C:/Users/Dell/Documents/Mxcube/CPU_test_08_10_20/subfunction.c:12:22: warning: assignment from incompatible pointer type [-Wincompatible-pointer-types]
sendcyp3=&Encryptedtext[2];
^
C:/Users/Dell/Documents/Mxcube/CPU_test_08_10_20/subfunction.c:13:22: warning: assignment from incompatible pointer type [-Wincompatible-pointer-types]
sendcyp4=&Encryptedtext[3];
^
C:/Users/Dell/Documents/Mxcube/CPU_test_08_10_20/subfunction.c: In function 'keypadfunction':
C:/Users/Dell/Documents/Mxcube/CPU_test_08_10_20/subfunction.c:437:31: warning: format '%X' expects argument of type 'unsigned int', but argument 3 has type 'uint32_t {aka long unsigned int}' [-Wformat=]
sprintf(display1,"%02X", eepromread_data);
~~~^
%02lX
C:/Users/Dell/Documents/Mxcube/CPU_test_08_10_20/subfunction.c: In function 'serial_print':
C:/Users/Dell/Documents/Mxcube/CPU_test_08_10_20/subfunction.c:1225:30: warning: comparison between pointer and integer
for(uint8_t i=0;i<string[i]!=NULL;i++)
^~
C:/Users/Dell/Documents/Mxcube/CPU_test_08_10_20/subfunction.c:1225:20: warning: suggest parentheses around comparison in operand of '!=' [-Wparentheses]
for(uint8_t i=0;i<string[i]!=NULL;i++)
~^~~~~~~~~~
C:/Users/Dell/Documents/Mxcube/CPU_test_08_10_20/pulser_data.c:191:29: warning: format '%X' expects argument of type 'unsigned int', but argument 3 has type 'uint32_t {aka long unsigned int}' [-Wformat=]
sprintf(buffer,"%08X", Plaintext[0]);
~~~^ ~~~~~~~~~~~~
%08lX
../Core/Inc/STM_MY_LCD16X2.h:57:13: warning: 'LCD1602_EnablePulse' declared 'static' but never defined [-Wunused-function]
static void LCD1602_EnablePulse(void);
^~~~~~~~~~~~~~~~~~~
../Core/Inc/STM_MY_LCD16X2.h:59:13: warning: 'LCD1602_RS' declared 'static' but never defined [-Wunused-function]
static void LCD1602_RS(bool state);
^~~~~~~~~~
../Core/Inc/STM_MY_LCD16X2.h:61:13: warning: 'LCD1602_write' declared 'static' but never defined [-Wunused-function]
static void LCD1602_write(uint8_t byte);
^~~~~~~~~~~~~
../Core/Inc/STM_MY_LCD16X2.h:63:13: warning: 'LCD1602_TIM_Config' declared 'static' but never defined [-Wunused-function]
static void LCD1602_TIM_Config(void);
^~~~~~~~~~~~~~~~~~
../Core/Inc/STM_MY_LCD16X2.h:64:13: warning: 'LCD1602_TIM_MicorSecDelay' declared 'static' but never defined [-Wunused-function]
static void LCD1602_TIM_MicorSecDelay(uint32_t uSecDelay);
^~~~~~~~~~~~~~~~~~~~~~~~~
../Core/Inc/STM_MY_LCD16X2.h:66:13: warning: 'LCD1602_writeCommand' declared 'static' but never defined [-Wunused-function]
static void LCD1602_writeCommand(uint8_t command);
^~~~~~~~~~~~~~~~~~~~
../Core/Inc/STM_MY_LCD16X2.h:68:13: warning: 'LCD1602_writeData' declared 'static' but never defined [-Wunused-function]
static void LCD1602_writeData(uint8_t data);
^~~~~~~~~~~~~~~~~
../Core/Inc/STM_MY_LCD16X2.h:70:13: warning: 'LCD1602_write4bitCommand' declared 'static' but never defined [-Wunused-function]
static void LCD1602_write4bitCommand(uint8_t nibble);
^~~~~~~~~~~~~~~~~~~~~~~~
I have attached the warning list as the snapshot.
2020-10-12 1:31 AM
What system hangs when you flash it? The entirety of STM32CubeIDE or the debug probe?
Is it only with this project or with every project you're trying to debug?
2020-10-12 4:03 AM
2020-10-20 12:01 AM
the problem is mainly due to sprintf function used in LCD header file and I have corrected it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.