2022-01-20 8:34 AM
I have an STM32F7 which I have configured RCC for and am using HSE as a clock source. When using the debugger trying to step through the generated code, my project is failing at the SystemClock_Config(), specifically:
/* Check the HSI ready flag */
if (__HAL_RCC_GET_FLAG(RCC_FLAG_HSIRDY) == RESET)
{
return HAL_ERROR;
}
}
I’ve done everything in the configurator and there are no errors in the pin configuration section. I have not added any code yet to the generated code, so I am not sure what is causing this error. The RCC configuration does show warnings with Master Clock Output 2 and Audio Clock Input, since I am using SDMMC1 and they conflict, but I don’t think I need those so I’m not sure if they are the source of the issue.
2022-01-21 1:44 AM
Hello @repairman
You said "I have configured RCC for and am using HSE as a clock source".
Are you sure you are using an external crystal?
/* HSI is selected as System Clock Source */
else
{
/* Check the HSI ready flag */
if (__HAL_RCC_GET_FLAG(RCC_FLAG_HSIRDY) == RESET)
{
return HAL_ERROR;
}
}
--> this part of code is related to HSI usage.
SofLit
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.