2021-08-31 3:17 PM
Can I have CubeIDE generate GPIO initialization that will be guarded by #if DEBUG?
On my board there are LEDs that are connected to pins which are also used for debugger connection. I want cube IDE to initialize those pins as outputs only if I set the project in Release build.
2021-08-31 4:11 PM
There are no user code sections defined within MX_GPIO_Init, somewhat surprisingly, so no you can't do this without the code being changed on regeneration.
CubeMX isn't really set up for multiple peripheral configurations.
2021-08-31 6:20 PM
Right,
I also think that it would make sense to have user code sections inside initialization function.
But this still wont be a solution for this problem.Lets say I have two pins PA1 and PA2, if I wan to to initialize PA1 in Debug build only, I will still be unable to solve this with user section only, because generated code will create one initialization code block for both pins as follows:
GPIO_InitStruct.Pin = GPIO_PIN_1 | GPIO_PIN_2; <--- here is a problem
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
Hopefully STM can add an option to generate code for each pin separate, and to add more user code sections in initialization code.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.