2025-10-15 2:37 AM - last edited on 2025-10-15 2:45 AM by Andrew Neil
Dear ST Support Team,
I am currently working with STM32CubeIDE and using the NUCLEO-H755ZITx development board. On one of the boards, I am consistently encountering the following error during debugging:
'filename_Debug' has encountered a problem. Error in final launch sequence. Failed to start GDB server.
I have attached a screenshot of the error for your reference.
This issue is blocking my development progress, and I would appreciate it if you could help me understand the root cause and suggest a resolution at the earliest.
Thank you for your support.
Best regards,
Prathiksha H L
2025-10-15 2:42 AM
Hello @Prathiksha ,
First let me thank you for posting and welcome to the ST Community.
For more investigation, could you provide please your project and the debug configuration tab.
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-10-15 3:08 AM
i Mahmoud,
For better clarity, let me share an example from our recent test. We attempted a simple LED blinking project using the STM32CubeIDE with the NUCLEO-H755ZITx board (Just to check the normality). After generating the code, I successfully upgraded the ST-LINK firmware (screenshot attached).
However, when I try to run or debug the code, I consistently encounter the following error:
'filename_Debug' has encountered a problem. Error in final launch sequence. Failed to start GDB server.
This is the same issue I mentioned in my previous email, and I’ve attached the relevant screenshot there.
Please let me know if you need any specific logs, configuration files, or further details to assist with your investigation.
I would appreciate your response as soon as possible, as this is blocking our development.
Best regards,
Prathiksha H L
2025-10-16 1:24 AM
Hello @Prathiksha ,
As discussed through the Chat, the issue is related to the dysfunctionality of your board and not to the STM32CubeIDE because you are able to debug other boards NUCLEO-H755ZITx with the same settings.
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-10-16 2:29 AM
Okay, let me be clear, our board is nothing but that one NUCLEO-H755ZITx is not working is what I mean.
and other NUCLEO-H755ZITx are working.
2025-10-22 2:18 AM
Hello @Prathiksha ,
Further to your comment, I can confirm that the issue is related to your board not to STM32CubeIDE.
Before launching the debug session, you can try to connect the board with STM32CubeProgrammer.
I suggest that you run tests on a functional board.
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.